Skip to main content
PMort.1
Associate
June 11, 2020
Question

STM32MP157 FMC NAN,D NCE or NCE2 ?

  • June 11, 2020
  • 1 reply
  • 1196 views

I want to connect a SLC NAND to the FMC controller and boot from it

What CS* must i use (NCE or NCE2) ?

Why i got the "Pin not available for boot step" in CUBEmx when trying to select NCE2 ?

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
June 11, 2020

Hello,

only SLC NAND device connected using FMC_NCE is supported as boot source.

You could refer to related wiki page and AN5031.

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent