cancel
Showing results for 
Search instead for 
Did you mean: 

OpenAMP_TTY_echo_wakeup example prevents A7 processor from going into low power mode.

nlbutts
Associate II

I'm trying to develop an application that puts the A7 into a low power mode and only uses the M4 to do some basic processing. I'm starting with the OpenAMP_TTY_echo_wakeup example. In the example it says to issue the following commands:

echo "*delay" >/dev/ttyRPMSG0

echo mem > /sys/power/state

Then after 20 seconds, the M4 will wake-up the A7. But when I have ANY M4 program running and I issue a:

echo mem > /sys/power/state

I get the following error messages;

root@stm32mp1:~# [ 1008.496994] PM: suspend entry (s2idle)

[ 1008.499292] PM: Syncing filesystems ... done.

[ 1008.509780] Freezing user space processes ... (elapsed 0.045 seconds) done.

[ 1008.560707] OOM killer disabled.

[ 1008.563608] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.

[ 1008.571108] Suspending console(s) (use no_console_suspend to debug)

[ 1008.633238] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget

[ 1008.633257] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0

[ 1008.633267] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0

[ 1008.698329] stm32-dma 48001000.dma: Suspend is prevented by Chan 1

[ 1008.698362] dpm_run_callback(): platform_pm_suspend+0x0/0x48 returns -16

[ 1008.698373] PM: Device 48001000.dma failed to suspend: error -16

[ 1008.698383] PM: Some devices failed to suspend, or early wake event detected

[ 1008.709397] dwmac4: Master AXI performs any burst length

[ 1008.709429] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found

[ 1008.751562] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget

[ 1009.294489] OOM killer enabled.

[ 1009.297551] Restarting tasks ... done.

[ 1009.316305] PM: suspend exit

[ 1012.901203] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx

If I reboot and attempt to enter low power mode, it succeds, but it will always fail after I start or start then stop an M4 program.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @nlbutts​ 

Please have a look to this page.

https://wiki.st.com/stm32mpu/wiki/Power_overview#How_to_enter_and_exit_low-power_modes

I suspect problem is that you are running in weston ..

You have to call 'systemctl suspend' instead of 'echo mem > /sys/power/state'

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
ST Employee

Note that the Readme file of the OpenAMP_TTY_echo_wakeup example will be update accordingly in next Cube package release.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
nlbutts
Associate II

I get the same issue. I suspect DMA1 is used to transfer data back and forth through OpenAMP.

root@stm32mp1:/usr/local/Cube-M4-examples# systemctl suspend

root@stm32mp1:/usr/local/Cube-M4-examples# [ 1882.992002] unbind driver brcmfmac/sdmmc

[ 1883.035445] brcmfmac: brcmf_fil_cmd_data: bus is down. we have nothing to do.

[ 1883.041748] brcmfmac: brcmf_fil_cmd_data: bus is down. we have nothing to do.

[ 1883.048704] brcmfmac: brcmf_cfg80211_get_channel: chanspec failed (-5)

[ 1883.237082] mmc1: card 0001 removed

[ 1883.241175] mmci-pl18x 58007000.sdmmc: Dropping the link to regulator.8

[ 1883.307366] PM: suspend entry (s2idle)

[ 1883.309665] PM: Syncing filesystems ... done.

[ 1883.378466] Freezing user space processes ... (elapsed 0.002 seconds) done.

[ 1883.386122] OOM killer disabled.

[ 1883.389272] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.

[ 1883.396895] Suspending console(s) (use no_console_suspend to debug)

[ 1883.467972] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget

[ 1883.467992] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0

[ 1883.468002] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0

[ 1883.513017] stm32-dma 48001000.dma: Suspend is prevented by Chan 1

[ 1883.513050] dpm_run_callback(): platform_pm_suspend+0x0/0x48 returns -16

[ 1883.513061] PM: Device 48001000.dma failed to suspend: error -16

[ 1883.525092] PM: Some devices failed to suspend, or early wake event detected

[ 1883.536067] dwmac4: Master AXI performs any burst length

[ 1883.536096] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found

[ 1883.576044] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget

[ 1884.119183] OOM killer enabled.

[ 1884.122249] Restarting tasks ... done.

[ 1884.131236] PM: suspend exit

[ 1884.218126] bind driver brcmfmac/sdmmc

[ 1884.221743] mmci-pl18x 58007000.sdmmc: allocated mmc-pwrseq

[ 1884.228474] mmci-pl18x 58007000.sdmmc: Linked as a consumer to regulator.8

[ 1884.234189] mmci-pl18x 58007000.sdmmc: mmc1: PL180 manf 53 rev1 at 0x58007000 irq 59,0 (pio)

[ 1884.293441] mmc1: queuing unknown CIS tuple 0x80 (2 bytes)

[ 1884.326662] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)

[ 1884.347891] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)

[ 1884.374922] mmc1: queuing unknown CIS tuple 0x80 (7 bytes)

[ 1884.381893] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)

[ 1884.395514] mmc1: queuing unknown CIS tuple 0x80 (6 bytes)

[ 1884.487706] mmc1: new high speed SDIO card at address 0001

[ 1884.504494] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1

[ 1884.675378] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1

[ 1884.745393] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM43430/1 wl0: Sep 11 2018 09:22:09 version f

[ 1887.675918] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx