Confused about BK1_NCS and BK2_NCS on STM32H750B-DK
On the STM32MP1, when booting from serial NOR flash, the STM32 MPU Wiki states "In dual mode, BK1_NCS shall be connected to BK2_NCS on board." Should MPU BK1_NCS and BK2_NCS GPIOs actually be connected, or rather is BK2_NCS GPIO unused?
I'm just confused since other kits (ex: STM32H750B-DK) have provisions for jumping the 2 lines together, but the wiki does not indicate the BK2_NCS GPIO (from the MPU) is even used by the BootROM. I wanted clarification of the statement made on the wiki article, mainly to be sure that shorting the BK1_NCS and BK2_NCS lines weren't required to put the QuadSPI in dual-bank mode. The statement on the wiki might be misleading.