Solved
How to specify the address to load Cortex-M4 firmware?
I want to know how to specify the address to load Cortex-M4 firmware when U-Boot or Linux Kernel load the firmware of Cortex-M4 in Retention RAM.
And, how to specify the address to load Cortex-M4 firmware if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately?
In addition, if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately, is the swithing of RetentionRAM and MCUSRAM done by MPU without the programmer being aware of it?