Skip to main content
GNapo.1
Associate
November 12, 2020
Question

How to do the synchronization between A7 and M4 using IPCC interrupt?

  • November 12, 2020
  • 9 replies
  • 2244 views

I would syncrhonize A7 and M4 on STM32MP151A using IPCC interrupt, how can I do it?

Moreover, using FreeRTOS, I need to start some task before of MX_OPENAMP_Init, but I noticed if I move this function after the Kernel starting, it doesn't work. I don't understand why?

This topic has been closed for replies.

9 replies

OlivierK
ST Technical Moderator
November 17, 2020

Have you tried to use OpenAMP examples provided inside the STM32Cube_FW_MP1 software package release? (Application/OpenAMP). Some examples are given to exercise FreeRTOS and OpenAMP which initialises/configures IPCC events.

Here's the entrypoint. https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_Package

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GNapo.1
GNapo.1Author
Associate
November 20, 2020

Hi Olivier,

thank you for the response.

I looked to entrypoint but it doesn't resolve my troubles. Due to in Openamp init the rproc_virtio_wait_remote_ready is blocking until Linux wakes up and due to some functionalities need to start before of Linux, I would manage the init of library in a separate task while another task containing the cited functionalities runs without waiting Linux.

I noticed that I moved the openamp initialization when Linux starts this task is blocked on waiting yet while the others starts fine, but I don't understand the reason of that. Is it possible that starting the FreeRTOS kernel before the OpenAmp init then it changes some memory areas where M4 expects to read the status from A7? How can I do it?

OlivierK
ST Technical Moderator
November 20, 2020

​Hi GNapo.1 (Community Member)

It seems that your are experiencing a similar issue as described in the following post:

https://community.st.com/s/question/0D53W000004l5HJ/openamp-hangs-at-mxopenampinit-when-started-from-uboot-even-after-waited-for-linux-to-fully-booted-up

Could you please have a look at it and let me know if it solves your problem?

Best Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GNapo.1
GNapo.1Author
Associate
November 24, 2020

Hi Oliver,

thank again. I saw the post but resource table is found, but investigating I noticed that in the MX_OPENAMP_Init function it returns -1 after executing

vdev = rproc_virtio_create_vdev(RPMsgRole, VDEV_ID, &rsc_table->vdev,

                 rsc_io, NULL, MAILBOX_Notify, NULL);

 if (vdev == NULL)

 {

  return -1;

 }

It is strange because the function seems is not able to allocate dynamically vdev. How it is possible?

I have scheduled the MX_OPENAMP_Init inside StartDefaultTask

 defaultTaskHandle = osThreadNew(StartDefaultTask, NULL,NULL);

Best Regards,

Giuseppe

GNapo.1
GNapo.1Author
Associate
November 30, 2020

Hi @OlivierK​ ,

do you have news for about that?

Thank you in advance.

King Regards

OlivierK
ST Technical Moderator
December 2, 2020

​Hi GNapo.1 (Community Member),

I am not able to reproduce. It seems your having an issue during the memory allocation . Have you tried to increase the heap/stack config sizes?

Kind Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GNapo.1
GNapo.1Author
Associate
December 2, 2020

Hi Olivier,

thanks.

Do you mean heap\stack of FreeRtos or in linker file of M4?

King Regards.

OlivierK
ST Technical Moderator
December 2, 2020

​Hi GNapo.1 (Community Member)

The problem may come from the allocated shared memory for OPENAMP defined in the linker file.

MEMORY

{

m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000298

m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000

m_data (RW) : ORIGIN = 0x10020000, LENGTH = 0x00020000

m_ipc_shm (RW) : ORIGIN = 0x10040000, LENGTH = 0x00008000

}

As in the OpenAMP_FreeRTOS_echo example, can you make sure you haven't modified this?

Kind Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GNapo.1
GNapo.1Author
Associate
December 3, 2020

Hi @OlivierK​ ,

this is my linker file

/* Highest address of the user mode stack */

_estack = 0x10040000;  /* end of RAM */

_Min_Heap_Size = 0x200 ; /* required amount of heap */

_Min_Stack_Size = 0x400 ; /* required amount of stack */

/* Memories definition */

MEMORY

{

 m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000298

 m_text    (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000

 m_data    (RW) : ORIGIN = 0x10020000, LENGTH = 0x00020000

 m_ipc_shm  (RW) : ORIGIN = 0x10040000, LENGTH = 0x00008000

}

 /* Symbols needed for OpenAMP to enable rpmsg */

__OPENAMP_region_start__ = ORIGIN(m_ipc_shm);

__OPENAMP_region_end__ = ORIGIN(m_ipc_shm)+LENGTH(m_ipc_shm);

Today I will try to increase the heap\stack size as you said in the previous response. I will give you a feedback.

King Regards.