Skip to main content
zxiao.4
Associate III
August 11, 2022
Question

Hi: I can't find qmake in 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15. When I use qtcreater5.15, I can't create STM32 code.

  • August 11, 2022
  • 1 reply
  • 979 views

When I use cmake,

/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/share/cmake-3.22/Modules/CMakeTestCXXCompiler.cmake:62: error: The C++ compiler "/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-g++" is not able to compile a simple test program. It fails with the following output: Change Dir: /home/zxb/qt_proj/build-untitled1-Stm32mp1-Debug/CMakeFiles/CMakeTmp Run Build Command(s):/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/ninja cmTC_1f845 && [1/2] Building CXX object CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o [2/2] Linking CXX executable cmTC_1f845 FAILED: cmTC_1f845 : && /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-g++ --sysroot=/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -O2 -pipe -g -feliminate-unused-debug-types -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o -o cmTC_1f845  && : /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/11.2.0/real-ld: error: cmTC_1f845 uses VFP register arguments, CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o does not /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/11.2.0/real-ld: failed to merge target specific data of file CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o collect2: error: ld returned 1 exit status ninja: build stopped: subcommand failed.

I got this...​How can I configure Qtcreator to work normally?

​

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
September 1, 2022

Hi @zxiao.4​ ,

Not sure it will fix your problem but please update to 4.0.2 release and let us know if you still have issue

OpenSTLinux Distribution patch release V4.0.2 is available

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.