Skip to main content
Associate II
November 26, 2023
Solved

FDCAN can not start, no clock found

  • November 26, 2023
  • 9 replies
  • 5822 views

after follow the wiki, the can0(m_can2) can not start up on stm32mp157d-dk1

root@stm32mp1:~# dmesg | grep can
[ 0.384348] can: controller area network core
[ 0.384666] can: raw protocol
[ 0.384678] can: broadcast manager protocol
[ 0.384695] can: netlink gateway - max_hops=1
[ 0.663370] m_can_platform 4400f000.can: no clock found

 

root@stm32mp1:~# cat /sys/kernel/debug/clk/clk_summary | grep fdcan
fdcan_k 0 0 0 74250000 0 0 50000 N
fdcan 0 0 0 104438965 0 0 50000 N

This topic has been closed for replies.
Best answer by Erwan SZYMANSKI

Hello @Huibean ,
With taking a better look at your device tree, I see that you include stm32mp157a-dk1-scmi.dtsi.

I ask myself, as this file has been made to configure only IPs that are on the board in question, I think the configuration for m_can2 is missing in your own case.

Can you please add this into the file, and tell me if it corrects something :

 

&m_can2 {
	clocks = <&scmi_clk CK_SCMI_HSE>, <&rcc FDCAN_K>;
};

 

Kind regards,
Erwan.

9 replies

Erwan SZYMANSKI
ST Technical Moderator
November 28, 2023

Hello @Huibean,
What gives you the following command :
Board $> cat /sys/kernel/debug/clk/clk-summary 

Moreover, can you show us how did you configure your device tree for can node ?(cf: https://wiki.stmicroelectronics.cn/stm32mpu/wiki/FDCAN_device_tree_configuration)

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HuibeanAuthor
Associate II
November 28, 2023

I have the clk_summary output like blew, full opuput need to get it tomorrow, the device tree are posted in the file

 

root@stm32mp1:~# cat /sys/kernel/debug/clk/clk_summary | grep fdcan
fdcan_k 0 0 0 74250000 0 0 50000 N
fdcan 0 0 0 104438965 0 0 50000 N

 

by decode the dtb I can get content like below

 

can@4400f000 {
compatible = "bosch,m_can";
reg = <0x4400f000 0x400 0x44011000 0x2800>;
reg-names = "m_can\0message_ram";
interrupts = <0x00 0x14 0x04 0x00 0x16 0x04>;
interrupt-names = "int0\0int1";
clocks = <0x0b 0x00 0x0b 0x9d>;
clock-names = "hclk\0cclk";
bosch,mram-cfg = <0x1400 0x00 0x00 0x20 0x00 0x00 0x02 0x02>;
feature-domains = <0x24 0x3e>;
status = "okay";
pinctrl-names = "default\0sleep";
pinctrl-0 = <0x5f>;
pinctrl-1 = <0x60>;
phandle = <0xd7>;
};

updated:

full clk_summary in file

 

Erwan SZYMANSKI
ST Technical Moderator
December 8, 2023

Hello,
This topic has been answered on this link : https://community.st.com/t5/stm32-mpus-products/no-clock-found-for-fdcan-stm32mp157d-dk1/m-p/612096

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.