Skip to main content
ABala.7
Visitor II
April 26, 2023
Solved

Does STM32MP153 and STM32MP157 support ECC for RAM interface ( DDR3)?

  • April 26, 2023
  • 2 replies
  • 1799 views

..

This topic has been closed for replies.
Best answer by Alex - APMemory

Hi, 

I'd like to comment about ECC DDR3. This device can be used with standard SoC. 

Please see below example based on Zentel Japan PN A3T4GF40CBF, 4Gb Built-in ECC DDR3/DDR3L SDRAM:

The ECC is a built-in function, the product has the features listed below

  • /DED (Double bit Error Detection) pin sends a fault detection signal to notify SoC of memory data error
  • Compatible with conventional JEDEC standard DRAM;
  • /DED pin is connected or unconnected does not affect ECC function;
  • /DED pin state or level does not affect ECC function
  • Note : Use Burst Chop and Data Mask may restrict the ECC functionality

Note:

  • /DED pin should be terminated at the VTTD and will be output low level when DED occurs.
  • If you do not use the DED notification, please fix /DED to VSS or OPEN.

AlexAPMemory_0-1697018807460.png

Alex

 

2 replies

PatrickF
ST Employee
April 27, 2023

Hi @ABala.7​ 

There is no support of DDR ECC on STM32MP1 products.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Alex - APMemory
Alex - APMemoryBest answer
Associate II
October 11, 2023

Hi, 

I'd like to comment about ECC DDR3. This device can be used with standard SoC. 

Please see below example based on Zentel Japan PN A3T4GF40CBF, 4Gb Built-in ECC DDR3/DDR3L SDRAM:

The ECC is a built-in function, the product has the features listed below

  • /DED (Double bit Error Detection) pin sends a fault detection signal to notify SoC of memory data error
  • Compatible with conventional JEDEC standard DRAM;
  • /DED pin is connected or unconnected does not affect ECC function;
  • /DED pin state or level does not affect ECC function
  • Note : Use Burst Chop and Data Mask may restrict the ECC functionality

Note:

  • /DED pin should be terminated at the VTTD and will be output low level when DED occurs.
  • If you do not use the DED notification, please fix /DED to VSS or OPEN.

AlexAPMemory_0-1697018807460.png

Alex