2023-04-03 8:11 AM
Hello,
Using a custom board loosely based on STM32mp157F-DK2
we are using boot0 and boot2 pins.According to documentation,
boot mode configuration is as follows;
Boot Mode BOOT2 BOOT0
Recov/DFU 0 0
Nor 0 1
Reserved(DEV) 1 0
SD-Card 1 1
Whereas with our board,I get a table like this
Boot Mode BOOT2 BOOT0
DFU 0 0
DFU 0 1
Reserved(DEV) 1 0
DFU 1 1
Since the board is in perpetual DFU mode I can't
boot from SD-card. Our HW engineer assured me that the
boot pins are connected correctly (1K resistors through VDD and dip switches)
Is there a way to force the board to boot from SD-card in that case
or is there something else that I might be missing?
Thanks in advance,
Solved! Go to Solution.
2023-04-03 9:08 AM
Hi,
If BootROM does not found a valid FSBL in SD-Card, there is a fall back in DFU.
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Boot_device_selection
So, your SD-Card is either not reachable (HW issue) or it's content is not well formed
check
You could also check BootROM trace to get more insight on what going wrong https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer
Regards.
2023-04-03 9:08 AM
Hi,
If BootROM does not found a valid FSBL in SD-Card, there is a fall back in DFU.
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Boot_device_selection
So, your SD-Card is either not reachable (HW issue) or it's content is not well formed
check
You could also check BootROM trace to get more insight on what going wrong https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer
Regards.
2023-04-04 7:46 AM
Hi there,
Ok BootRom falling back to USB boot mode has opened a can of worms for me.Although
it should be obvious since I've read that wiki page countless times.Somehow I'd always
thought DFU is something different from Serial boot. I've checked with DK2 board and
you are right.it falls back to DFU mode if sd card is removed from the board.
So let me explain my situation in a litte bit more detail with due consideration
with the points you have made.
I can download the tf-a and uboot binaries to the board using the DFU mode with
the a simple TSV file with help of STM32Programmer_CLI and can run FSBL and SSBL
Here is the console output of u-boot mmc commands
STM32MP> mmc list
STM32 SD/MMC: 0 (eMMC)
STM32 SD/MMC: 1 (SD)
STM32MP> mmc info
Device: STM32 SD/MMC
Manufacturer ID: 2
OEM: 544d
Name: SA08G
Bus Speed: 50000000
Mode: SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.2 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
As you can see the SD card is detected (I can also read the contents)
but you should also notice that the our configuration is different from the standard
configuration. We have a 8bit e-mmc at SDMMC1 and SD card at SDMMC2.DTS is
generated by STMCube from the ICO file and modified accordingly.
I've set the otp word 3 to 0x00000010 to set SD card memory interface to SDMMC2
but since our pinmux is different from "default pins" I have to set AFMUX configuration
as per https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Boot_from_SD_card
(it is coming together as I write this.)
AFMUX configuration seems arcane to me and I'm not sure how to set it up. Below is t
he pinmux configuration for SDMMC2 in our board.
sdmmc2_pins_mx: sdmmc2_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-pull-up;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-pull-up;
drive-push-pull;
slew-rate = <2>;
};
};l
Since Otp is one time (I've already bricked one board ) I need a little help as how to translate the pinmux to configuration words.Documentation about it non-existent and simple example would go beyond words.
As for ROM traces, ST-link port is not exposed to outside world for this revision so I can't check
but I've discussed this with our HW designer to include it in the next revision.
Thanks
2023-04-04 8:10 AM
Hi @Golgepapaz
to inform BootROM to use SD-Card over SDMMC2 CLK, CMD, D0 (sufficient for BootROM), respectively on pins PE3 PG6 and PB14, you should setup the following OTPs:
You could double check values above using https://wiki.st.com/stm32mpu/wiki/STM32MP15_OTP_mapping#AFmux_configuration
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-04-04 12:22 PM
Ok just to be sure I'm going to break down the OTP for SDMMC2_CK given by the definition
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-pull-up;
drive-push-pull;
slew-rate = <2>;
};5391 assuming LSB is rightmost bit
15-12 (4 bits) Bank id; 5 => E;
11-8 (4 bits) Pin id; 3 => 3;
7-4 (4 bits) AFmux value; 9 => AF9
3-0 (4 bits) Pin Mode ; 1 :AF, No pull, Medium speed => bias-pull-up
The same logic can be applied to other pins as well. Only difference is pin mode is set to 4 (AF, Pull up, Medium speed) for other pins. Is this deliberate? I'd expect this one would be set to 4 as well because of the bias-pull-up property in the DTS or it has to be this way since it's a clock signal.it's also strongly probable there is no relation between DTS property and pin mode as well.
Thanks in advance again.
Hurcan
2023-04-05 5:46 AM
Hi,
pull-up or not on SDMMC2 CLK should not make any difference for BootROM as it is push-pull during whole boot sequence.
Maybe useful for Device Tree as pin could de deallocated by Linux.
2023-04-06 4:39 AM
Board now boots from sd-card . Thank you for your help. though kernel fails to load with panic I'll make another post if I am unable to resolve it.