Skip to main content
kKim.1
Associate II
February 2, 2023
Solved

Can I install the developer package on the STM32MP157D-EV1 board using "Windows os" STM32Cubeprogrammer program?

  • February 2, 2023
  • 1 reply
  • 932 views

I even installed the starter package in EMMC boot mode.

And I want to install a developer package.

I want to install SDK, can I use STM32MP157D-EV1 board using STM32Cube Programmer in Windows OS?

Ubuntu 18.04 was installed in virtualbox and STM32Cubeprogrammer was installed. However, the program cannot read the STM32 board on the USB port.

I want to install Ubuntu 18.04 on the STM32MP157D-EV1 board. Is there any way?

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @kKim.1​ ,

There's no way to install Ubuntu 18.04 or SDK on the target board STM32MP157D-EV1.

It looks like you mixed Host / PCs requirement and ecosystem side and the target side.

On Host side : Ubuntu 20.04 LTS on which you can install developper package (SDK + source code) or Distribution ( Yocto)

Target side : Only support OpenSTLinux executable binaries cross-compiled on you PCs thanks to Developper or Distribution package and download with STM32CubeProg on your boot device (eMMC, SDCard et.. )

Hope it help,

Olivier

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 2, 2023

Hi @kKim.1​ ,

There's no way to install Ubuntu 18.04 or SDK on the target board STM32MP157D-EV1.

It looks like you mixed Host / PCs requirement and ecosystem side and the target side.

On Host side : Ubuntu 20.04 LTS on which you can install developper package (SDK + source code) or Distribution ( Yocto)

Target side : Only support OpenSTLinux executable binaries cross-compiled on you PCs thanks to Developper or Distribution package and download with STM32CubeProg on your boot device (eMMC, SDCard et.. )

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.