Skip to main content
AKuma.46
Associate II
November 21, 2022
Question

Building and deploying the Linux kernel for the first time. command- make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 O="$PWD/../build"

  • November 21, 2022
  • 4 replies
  • 1922 views

*** The source tree is not clean, please run 'make ARCH=arm mrproper'

*** in /home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10

***

make[2]: *** [outputmakefile] Error 1

make[1]: *** [/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10/include/config/auto.conf.cmd] Error 2

make[1]: Leaving directory `/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build'

make: *** [__sub-make] Error 2

This topic has been closed for replies.

4 replies

Olivier GALLIEN
ST Technical Moderator
November 22, 2022

Hi @AKuma.46​ 

There can be multiple reasons to reach this point :

*** The source tree is not clean, please run 'make ARCH=arm mrproper'

Did you follow wiki and/or README instructions?

You can either try the recommended mrproper ...or restart from a fresh installation.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AKuma.46
AKuma.46Author
Associate II
November 25, 2022

Dear @Community member​ 

Thanks for you valuable suggestion, after mrproper this error was resolved. but again came to new error:

cc1: error: cannot load plugin ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so

  ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: undefined symbol: _ZN8opt_pass14set_pass_paramEjb

make[2]: *** [scripts/mod/empty.o] Error 1

make[1]: *** [prepare0] Error 2

make[1]: Leaving directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build'

make: *** [__sub-make] Error 2

Please let me know what's the root of this issue.

Note:

ggc installed version is "gcc (Ubuntu 8.4.0-3ubuntu2) 8.4.0" and Ubuntu version is 20.04

Thanks & Regards

Aniket Kumar

Olivier GALLIEN
ST Technical Moderator
November 25, 2022

Hi @AKuma.46​ ,

>> gc installed version is "gcc (Ubuntu 8.4.0-3ubuntu2) 8.4.0" 

this is not good and probably root cause as it highlights you probably omit to source the SDK.

Please refer to :

Install the SDK - stm32mpu

With a correct environnement setup you might get something like :

$CC --version

arm-ostl-linux-gnueabi-gcc (GCC) 11.3.0

Copyright (C) 2021 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AKuma.46
AKuma.46Author
Associate II
November 25, 2022

Dear @Community member​ 

We downloaded YOCTO SDK version 3.0.0 and Developer Package 3.0.0 and found gcc version is 9.3.0, please find the details below.

DEVELOPER PACKAGE DETAILS

aniket.kumar@si-rd22:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ source /developer-package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

aniket.kumar@si-rd22:~p/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ set |grep CROSS

CROSS_COMPILE=arm-ostl-linux-gnueabi-

aniket.kumar@si-rd22:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ $CC --version

arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0

Copyright (C) 2019 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

YOCTO SDK DETAILS

aniket.kumar@si-rd22:~/developer-package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-li              nux-gnueabi$ ./arm-ostl-linux-gnueabi-gcc --version

arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0

Copyright (C) 2019 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

As both YOCTO SDK and Developer package SDK is of same version still we are facing this issue while building linux kernel build.

aniket.kumar@si-rd22-bld72:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linustm32mp-5.10.10-r0/linux-5.10.10$ make ARCH=arm modules O="$PWD/../build"

make[1]: Entering directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostlinux-gnueabi/linux-stm32mp-5.10.10-r0/build'

 GEN   Makefile

 CC   scripts/mod/empty.o

cc1: error: cannot load plugin ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so

  ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: undefined symbol: _ZN8opt_pass14set_pass_paramEjb

make[2]: *** [scripts/mod/empty.o] Error 1

make[1]: *** [prepare0] Error 2

make[1]: Leaving directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-nux-gnueabi/linux-stm32mp-5.10.10-r0/build'

make: *** [__sub-make] Error 2

Thankyou