2025-04-24 6:14 PM - last edited on 2025-05-06 5:16 AM by Andrew Neil
We are currently developing a demo product using the STM32MP257F-DK board.
We have flashed the firmware using the file .images\stm32mp25-disco\flashlayout_st-image-core\optee\FlashLayout_emmc_stm32mp257f-dk-optee.tsv
However, we found that the USB DRD port (CN15) is not being recognized.
Upon checking the device tree source in the kernel, we observed that the USB3DR functionality appears to be controlled via , suggesting that an MCU may be required for this functionality.i2c_rpmsg
We would like to confirm the following:
We would greatly appreciate your guidance or reference to any relevant documentation, firmware examples, or configuration tips.
[Please paste the URL here]
USB3DR device tree configuration - stm32mpu
USB3DR internal peripheral - stm32mpu
COMBOPHY device tree configuration - stm32mpu
UCPD internal peripheral - stm32mpu
OTG device tree configuration - stm32mpu
Linux RPMsg framework overview - stm32mpu
Solved! Go to Solution.
2025-05-06 5:14 AM - edited 2025-05-06 5:26 AM
We are also facing the same issues with the STM32MP257F-EV1 board, as we intend to use the M33 core to perform other functions.
We have found a guide to force "peripheral-only" working mode, but is sub-optimal as it is not following the USB standard (VBUS and ID are not properly handled): https://wiki.stmicroelectronics.cn/stm32mpu/wiki/USB3DR_device_tree_configuration#DT_configuration_example_as_USB2-speed_only_USB3DR_in_Peripheral_mode--with_micro-B-28ID_left_unconnected-29_or_Type-C_connector
We also have tested the combination suggested in: https://wiki.stmicroelectronics.cn/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_high_speed_OTG.2C_with_micro-B_connector.2C_Vbus_and_ID_mapped_on_GPIOs
But in this case, the configuration not only didn't enabled the "read" of OTG pins (VBUS - ID) but also rendered the USB_DRD port unresponsive to connections. Also when connecting with the UMS function of U-BOOT, the only configuration that work is the following with maximum-speed = "full-speed":
https://wiki.stmicroelectronics.cn/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#On_STM32MP2-lines_and_STM32MP2-lines
As with the suggested maximum-speed = "high-speed" it fails to mount as scsi unit in Unbuntu 20.04, even if it is correctly recognised as a "USB download gadget".
Thank you for any help
2025-05-06 5:14 AM - edited 2025-05-06 5:26 AM
We are also facing the same issues with the STM32MP257F-EV1 board, as we intend to use the M33 core to perform other functions.
We have found a guide to force "peripheral-only" working mode, but is sub-optimal as it is not following the USB standard (VBUS and ID are not properly handled): https://wiki.stmicroelectronics.cn/stm32mpu/wiki/USB3DR_device_tree_configuration#DT_configuration_example_as_USB2-speed_only_USB3DR_in_Peripheral_mode--with_micro-B-28ID_left_unconnected-29_or_Type-C_connector
We also have tested the combination suggested in: https://wiki.stmicroelectronics.cn/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_high_speed_OTG.2C_with_micro-B_connector.2C_Vbus_and_ID_mapped_on_GPIOs
But in this case, the configuration not only didn't enabled the "read" of OTG pins (VBUS - ID) but also rendered the USB_DRD port unresponsive to connections. Also when connecting with the UMS function of U-BOOT, the only configuration that work is the following with maximum-speed = "full-speed":
https://wiki.stmicroelectronics.cn/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#On_STM32MP2-lines_and_STM32MP2-lines
As with the suggested maximum-speed = "high-speed" it fails to mount as scsi unit in Unbuntu 20.04, even if it is correctly recognised as a "USB download gadget".
Thank you for any help