Skip to main content
Dat Tran
Senior II
March 9, 2023
Question

STM32MP151 change default UART

We want to change default uart from UART4 to UART8,

from:

aliases {

ethernet0 = &ethernet0;

serial0 = &uart4;

....

};

we changed

serial0 = &uart8;

and implement uart8 as below:

&uart8 {

pinctrl-names = "default", "sleep", "idle";

pinctrl-0 = <&uart8_pins_a>;

pinctrl-1 = <&uart8_sleep_pins_a>;

pinctrl-2 = <&uart8_idle_pins_a>;

status = "okay";

};

uart8_pins_a: uart8-0 {

pins1 {

pinmux = <STM32_PINMUX('E', 1, AF8)>; /* UART8_TX */

bias-disable;

drive-push-pull;

slew-rate = <0>;

};

pins2 {

pinmux = <STM32_PINMUX('E', 0, AF8)>; /* UART8_RX */

bias-disable;

};

};

uart8_idle_pins_a: uart8-1 {

pins1 {

pinmux = <STM32_PINMUX('E', 1, ANALOG)>; /* UART8_TX */

};

pins2 {

pinmux = <STM32_PINMUX('E', 0, AF8)>; /* UART8_RX */

bias-disable;

};

};

uart8_sleep_pins_a: uart8-2 {

pins {

pinmux = <STM32_PINMUX('E', 1, ANALOG)>, /* UART8_TX */

<STM32_PINMUX('E', 0, ANALOG)>; /* UART8_RX */

};

};

Is there anything else we should take a look, please?

This topic has been closed for replies.

1 reply

OlivierK
ST Technical Moderator
March 17, 2023

Hi Dat Tran (Community Member)

After changing the pin-muxing, you need to enable the UART8 status=okay in the DT board config for all the BSP DT (TF-A/U-boot/OP-TEE) and Kernel DT.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.