Skip to main content
uouox
Associate II
December 30, 2021
Question

Kernel panic during startup

  • December 30, 2021
  • 1 reply
  • 981 views

Hi I built the linux kernel by following the steps on the stm32mpu wiki web. All default configuration except enabled earlyprintk.

However, when I restart the system, it does not work any more.

This is the error in boot log.

...

[  0.349451] pps_core: LinuxPPS API ver. 1 registered

[  0.354493] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

[  0.363706] PTP clock support registered

[  0.368477] arm-scmi firmware:scmi0: SCMI Notifications - Core Enabled.

[  0.375147] 8<--- cut here ---

[  0.378218] Unhandled fault: external abort on non-linefetch (0x008) at 0xe081f004

[  0.385829] pgd = (ptrval)

[  0.388549] [e081f004] *pgd=c183c811, *pte=2ffff653, *ppte=2ffff453

[  0.394877] Internal error: : 8 [#1] PREEMPT SMP ARM

...

Any hint? The board is stm32mp157f-dk2

Thanks

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
January 4, 2022

Hi @uouox​ ,

Could you please elaborate further if you used Developer package or Distribution package for rebuild ?

What ecosystem / kernel version ?

Are you using default Device Tree as per delivered by ST ?

Thx

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.