Skip to main content
Associate
April 30, 2024
Question

Flashing error

  • April 30, 2024
  • 6 replies
  • 2099 views

I am currently flashing a custom mickledore distro on a STM32MP151CAA3T and after the fsbl1 i get this error :

ERROR: DDR addr bus test: can't access memory @ 0xc0000004

PANIC at PC : 0x2ffdf9d9

Can someone explain how to solve this issue?

This topic has been closed for replies.

6 replies

DBELL.1
ST Employee
April 30, 2024

Hello @Pavesino ,

 

The cube programmer attempts to program the external memories.

Did you have the partition 3 well programmed?

It seems the firmware in partition 3 is not properly loaded.
The purpose of this firmware is to initialize the external memory and then the cube programmer can use it.

 

regards,
David B.

PavesinoAuthor
Associate
April 30, 2024

How can i check if i well programmed the partition 3?

DBELL.1
ST Employee
April 30, 2024

Hello @Pavesino ,

 

Please, just check in the TSV file, what fip is used or if the line is missing.

 

rgds
David B

 

PavesinoAuthor
Associate
April 30, 2024

in the TSV for partition 3 i have 

fip/fip-stm32mp151c-epro-mx-optee.bin

so no missing line for this

thanks

DBELL.1
ST Employee
April 30, 2024

Hello @Pavesino ,

 

This bin seems to have a problem.

Do you have another one maybe with another board?

Do you have the same kind of problem while programming STM32MP157 board?

 

regards,
David B

PatrickF
ST Employee
April 30, 2024

HI @Pavesino 

Flashing is done by loading TF-A, which then init the DDR to load uBoot which is responsible for Flashing.

Here it seems TF-A is not able to see the DDR correctly working.

Probable issues (some could be detected by using DDRFW-UTIL tool :

  • Bad DDR configuration (did you use CubeMX to generate DDR settings?)
  • DDR supplies not started (did you use STPMIC1 ?)
  • PCB issue (bad connection in schematics, bad routing, etc...)
  • Manufacturing issue (soldering)
  • etc...

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent