2023-12-11 2:09 PM - edited 2023-12-11 2:11 PM
Hello,
currently, I'm in the production phase of my product which is based on stm32mp153. Unfortunately, I have a huge problem with setting the password for root.
First I commented debug-tweks in local.conf.
I added
INHERIT += "extrausers"
EXTRA_USERS_PARAMS = " \
usermod -p '$5$otifn3fxcID0nu0c$QUDR.mLMbgEgl26XPEX6Rm6ASUB0ab8UFtQHdoEOBt4' root; \
"
hashed or not based password but I can't login into root using ssh.
Then I discovered that I could still log in through the serial console without providing anything. I found and commented 'serial-getty@.service'
line
ExecStart=-/sbin/agetty -8 --autologin root -L --keep-baud %I @BAUDRATE@ $TERM
to
ExecStart=-/sbin/agetty -8 -L --keep-baud %I @BAUDRATE@ $TERM
Additionally, I updated sshd_config file line
PermitRootLogin prohibit-password
to
PermitRootLogin yes
And finally, the result is that I can't log in via serial and ssh.
I read some issues from the link
https://www.blaess.fr/christophe/yocto-lab/index.html
without success.
My intention is simple how to modify local.conf or any other file to login via ssh and serial on root using password.
PS. I discover also that the capital letter P cause a problem with st-image-weston compilation
usermod -P
Solved! Go to Solution.
2023-12-11 11:11 PM
2023-12-11 11:11 PM