Skip to main content
Associate III
July 25, 2024
Solved

STM32MP157 using qt5 issue

  • July 25, 2024
  • 2 replies
  • 1021 views

I used buildroot to build the root file system and encountered the following error while running the qt example:

penat(AT_FDCWD, "/dev/galcore", O_RDWR) = -1 ENOENT (No such file or directory)

openat(AT_FDCWD, "/dev/graphics/galcore", O_RDWR) = -1 ENOENT (No such file or directory) clock_nanosleep(CLOCK_REALTIME, 0, {tv_sec=1, tv_nsec=0}, 0xbe8ec8d0) = 0

write(2, "[ 1] Failed to open device: "..., 72) = 72

I loaded galcore.ko, but there are indeed no galcore and graphics/galcore under/dev/:

# dmesg | grep galcore

[ 9.490473] galcore: loading out-of-tree module taints kernel.

# ls /dev/galcore*

ls: /dev/galcore*: No such file or directory

I used tslib to test touch and modetest to test LCD, both of which were normal. Why does my Qt still not run properly?

This topic has been closed for replies.
Best answer by zengyixiang

Has anyone encountered this situation before?

2 replies

zengyixiangAuthorBest answer
Associate III
July 26, 2024

Has anyone encountered this situation before?

Associate III
July 29, 2024

Has anyone encountered this situation before?