Skip to main content
PPiwk.1
Associate II
February 2, 2024
Solved

STM32MP151C U-boot stucks after relocating

  • February 2, 2024
  • 2 replies
  • 2087 views

 

Hi there,

I currently work on the integration of OPTEE to our custom STM32MP151C-based platform. The problem that I've faced is that U-boot hangs just after the board_init_f() function and relocation procedure:

 

NOTICE: CPU: STM32MP151CAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board (TF-A)
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x8000000 (128 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c7146592
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff1fa
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
INFO: BL2: Loading image id 21
INFO: Loading image id=21 at address 0x2ffc0000
INFO: Image id=21 loaded: 0x2ffc0000 - 0x2ffd2628
INFO: BL2: Loading image id 22
INFO: Loading image id=22 at address 0xc6200000
INFO: Image id=22 loaded: 0xc6200000 - 0xc624d000
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0511fb0
INFO: BL2: Skip loading image id 26
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01d4c6c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc0000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Pager is enabled. Hashes: 2784 bytes
I/TC: Pager pool size: 60kB
I/TC: Non-secure external DT found
I/TC: Embedded DTB found
I/TC: OP-TEE version: 3.16.0-dev (gcc version 12.2.0 (GCC)) #19 Fri Jan 28 02:28:18 PM UTC 2022 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: DT clock tree configurations were ignored
I/TC: WARNING: All debug access are allowed
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151c-0068-new-1-mx.dts
I/TC: DTB enables console (non-secure)
I/TC: Primary CPU switching to normal world boot
...
U-Boot 2021.10-stm32mp-r1-dirty (Oct 04 2021 - 15:09:26 +0000)

U-Boot code: C0100000 -> C01BCBF4 BSS: -> C01C9568
psci psci: set_state_simple op missing
stm32mp_bsec efuse@5c005000: set_state_simple op missing
CPU: STM32MP151CAC Rev.Z
Model: STMicroelectronics custom STM32CubeMX (U-Boot)
Board: stm32mp1 in trusted mode (st,stm32mp151c-0068-new-linux-mx)
DRAM: stm32mp1_ddr ddr@5a003000: set_state_simple op missing
Monitor len: 000C9568
Ram size: 08000000
Ram top: C8000000
Reserving 805k for U-Boot at: c7f26000
Reserving 33024k for malloc() at: c5ee6000
Reserving 1M for noncached_alloc() at: c5d00000
Reserving 72 Bytes for Board Info at: c5cfffb0
Reserving 216 Bytes for Global Data at: c5cffed0
Reserving 72640 Bytes for FDT at: c5cee310

RAM Configuration:
Bank #0: c0000000
DRAM: 128 MiB
New Stack Pointer is: c5cee2f0
Relocation Offset is: 07e26000
Relocating to c7f26000, new gd at c5cffed0, sp at c5cee2f0

I guess the issue might be related to the incorrect memory mapping and potential overlaps. The only thing I changed compared to the previous well working configuration (non OPTEE based) was increasing CONFIG_SYS_MALLOC_F_LEN from 0x3000 to 0x40000 which solves the problem regarding to "alloc space exhausted" error.

I use the stm32mpu-ecosystem-v4 provided by the meta-st-stm32mp yocto layer (langdale).

Is there something I missed or have to configure in addition?

Thanks in advance for any hints!

 

 

This topic has been closed for replies.
Best answer by PatrickD

Hi,

in your trace, it seems the OP-TEE in loaded at address: 0xc6200000

INFO: Loading image id=22 at address 0xc6200000
INFO: Image id=22 loaded: 0xc6200000 - 0xc624d000

And U-Boot use the end of DDR (128 MiB) for relocation address with "Ram top: C8000000": 

 Relocating to c7f26000, new gd at c5cffed0, sp at c5cee2f0

So relocated U-Boot is clearly overridden the OP-TEE location.

Normally the OP-TEE reserved memory is preserved by U-Boot, when it is correctly configured in the U-Boot device tree.


Check in your device tree in U-Boot, if you have  the node with the correct address (I don't sure of the size with size of memory used by OP-TEE (you need crosscheck with OP-TEE configuration)

/ {
  reserved-memory {
    optee@c6200000 {
      reg = <0xc6200000 0x50000>;
      no-map;
    };
  };
};

See also  https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package#U-Boot_updates

As alternate dirty solution  (for test)

=> change in U-boot code the "ram top" value, it is the result of board_get_usable_ram_top() in arch/arm/mach-stm32mp/dram_init.c

return 0xc6200000;

And U-Boot willl be reloaded before OP-TEE location = 0xc6200000.

regards,

Patrick

2 replies

PatrickD
PatrickDBest answer
ST Employee
February 5, 2024

Hi,

in your trace, it seems the OP-TEE in loaded at address: 0xc6200000

INFO: Loading image id=22 at address 0xc6200000
INFO: Image id=22 loaded: 0xc6200000 - 0xc624d000

And U-Boot use the end of DDR (128 MiB) for relocation address with "Ram top: C8000000": 

 Relocating to c7f26000, new gd at c5cffed0, sp at c5cee2f0

So relocated U-Boot is clearly overridden the OP-TEE location.

Normally the OP-TEE reserved memory is preserved by U-Boot, when it is correctly configured in the U-Boot device tree.


Check in your device tree in U-Boot, if you have  the node with the correct address (I don't sure of the size with size of memory used by OP-TEE (you need crosscheck with OP-TEE configuration)

/ {
  reserved-memory {
    optee@c6200000 {
      reg = <0xc6200000 0x50000>;
      no-map;
    };
  };
};

See also  https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package#U-Boot_updates

As alternate dirty solution  (for test)

=> change in U-boot code the "ram top" value, it is the result of board_get_usable_ram_top() in arch/arm/mach-stm32mp/dram_init.c

return 0xc6200000;

And U-Boot willl be reloaded before OP-TEE location = 0xc6200000.

regards,

Patrick

PPiwk.1
PPiwk.1Author
Associate II
February 5, 2024

Hi PatrickD, 

As you suggested, my OPTEE node had the incorrect addresses set. 

Thank you