Skip to main content
SKim.12
Associate II
June 23, 2020
Solved

I have "ERROR: Function failed: do_compile". I want solve it. Please help me.

  • June 23, 2020
  • 1 reply
  • 1624 views

Hello dear.

​

I solved all errors and warnings.

But I am getting a do_compile error and I can't figure out the cause, so I need help.

I used the devtool build cherry0 command and bitbake cherry0 causes the same situation.

The build message is:

-------------------------------------------------------------------

moonlive@kheng:~/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/workspace$ devtool build cherry0

NOTE: Starting bitbake server...

NOTE: Started PRServer with DBfile: /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 42503, PID: 7602

WARNING: You have included the meta-gnome layer, but 'x11' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-gnome README for details on enabling meta-gnome support.

Loading cache: 100% |###########################################################################################################################| Time: 0:00:11

Loaded 3573 entries from dependency cache.

Parsing recipes: 100% |#########################################################################################################################| Time: 0:00:42

Parsing of 2529 .bb files complete (2525 cached, 4 parsed). 3574 targets, 396 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

​

Build Configuration:

BB_VERSION          = "1.40.0"

BUILD_SYS           = "x86_64-linux"

NATIVELSBSTRING     = "universal"

TARGET_SYS          = "arm-ostl-linux-gnueabi"

MACHINE             = "stm32mp1"

DISTRO              = "openstlinux-eglfs"

DISTRO_VERSION      = "2.6-snapshot-20200623"

TUNE_FEATURES       = "arm armv7ve vfp thumb neon vfpv4 callconvention-hard cortexa7"

TARGET_FPU          = "hard"

DISTRO_CODENAME     = "thud"

ACCEPT_EULA_stm32mp1 = "0"

GCCVERSION          = "8.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python         

meta-oe             

meta-oe             

meta-gnome          

meta-xfce           

meta-initramfs      

meta-multimedia     

meta-networking     

meta-webserver      

meta-filesystems    

meta-perl           

meta-python         = "HEAD:436cf0aa2b2802da706588d4daa1a8240d172df8"

meta-st-stm32mp     = "HEAD:8055ad11c92144e4a147a00834de53a2de21e42d"

meta-qt5            = "HEAD:1520d5b2b2beec5e1c3209d3178219e93ef08bca"

meta-st-openstlinux = "HEAD:f023f39b13fa13f6391be5fbc10fb2bf7369402a"

meta                = "HEAD:cd7cf933b3235560ec71576d8f3836dff736a39f"

workspace           = "<unknown>:<unknown>"

​

Initialising tasks: 100% |######################################################################################################################| Time: 0:00:01

Sstate summary: Wanted 4 Found 4 Missed 0 Current 114 (100% match, 100% complete)

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: cherry0: compiling from external source tree /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/workspace/cherry0

ERROR: cherry0-1.0-r0 do_compile: Function failed: do_compile (log file is located at /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cherry0/1.0-r0/temp/log.do_compile.7671)

ERROR: Logfile of failure stored in: /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cherry0/1.0-r0/temp/log.do_compile.7671

Log data follows:

| DEBUG: Executing python function externalsrc_compile_prefunc

| NOTE: cherry0: compiling from external source tree /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/workspace/cherry0

| DEBUG: Python function externalsrc_compile_prefunc finished

| DEBUG: Executing shell function do_compile

| WARNING: /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cherry0/1.0-r0/temp/run.do_compile.7671:1 exit 1 from 'arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=/home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cherry0/1.0-r0/recipe-sysroot *.cc -o cherry0'

| ERROR: Function failed: do_compile (log file is located at /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cherry0/1.0-r0/temp/log.do_compile.7671)

ERROR: Task (/home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/workspace/recipes/cherry0/cherry0.bb:do_compile) failed with exit code '1'

NOTE: Tasks Summary: Attempted 493 tasks of which 492 didn't need to be rerun and 1 failed.

NOTE: Writing buildhistory

​

Summary: 1 task failed:

 /home/moonlive/work/STM32MP1/Distribution-Package/openstlinux-20-02-19/build-openstlinuxeglfs-stm32mp1/workspace/recipes/cherry0/cherry0.bb:do_compile

Summary: There was 1 WARNING message shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

--------------------------------------------------------------------------------------------------

I want solve it. Please help me.

Thank you in advance.

This topic has been closed for replies.
Best answer by SKim.12

I solved this problem.

This is a problem in the process of building the source code that was executed on other existing hardware with STM32MP1.

When I was trying to build a devtool, I couldn't find out the contents of the fail, but when I built it in the developer package, I found the error and solved it

In conclusion, it was caused by a problem with the referenced library.

I solved the problem by building and referencing the library as STM32MP1.

1 reply

SKim.12
SKim.12AuthorBest answer
Associate II
June 24, 2020

I solved this problem.

This is a problem in the process of building the source code that was executed on other existing hardware with STM32MP1.

When I was trying to build a devtool, I couldn't find out the contents of the fail, but when I built it in the developer package, I found the error and solved it

In conclusion, it was caused by a problem with the referenced library.

I solved the problem by building and referencing the library as STM32MP1.