Skip to main content
jhi
Senior
January 7, 2022
Solved

Ethernet on STM32MP157A with PHY AR8035 no PHY found

  • January 7, 2022
  • 13 replies
  • 5593 views

I have a problem to get the ethernet to work with the PHY AR8035 (Atheros). The board is from MYiR (MYC-YA157C-V2), but they are only providing yocto based image and I'm doing my work with buildroot. I'm using the bootlin buildroot branch: st/2021.02 https://github.com/bootlin/buildroot.git

The kernel can't find MDIO: mdio_bus stmmac-0: MDIO device at address 6 is missing.

The funny thing is, if I first boot the board from eMMC where the original image from MYiR is flashed, and afterwards, without switching power off, I start my image from the sdcard, the ethernet works. I guess this means that some register value is wrong, but I don't know where to start look. This also means that address 6 for the MDIO is also correct.

On TF-A I have CLK_ETH_DISABLED, because the 125MHz is coming from the PHY.

Below is the device tree for the kernel (CONFIG_AT803X_PHY=y is set):

&ethernet0 {
	interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
						<&intc GIC_SPI 62 IRQ_TYPE_LEVEL_HIGH>,
						<&exti 70 1>;
	interrupt-names = "macirq",
				"eth_wake_irq",
				"stm32_pwr_wakeup";
 
	clock-names = "stmmaceth",
				"mac-clk-tx",
				"mac-clk-rx",
				"eth-ck",
				"ethstp";
 
	clocks = <&rcc ETHMAC>,
			<&rcc ETHTX>,
			<&rcc ETHRX>,
			<&rcc ETHCK_K>,
			<&rcc ETHSTP>;
					
	status = "okay";
	pinctrl-0 = <&eth1_pins_mx>;
	pinctrl-1 = <&eth1_sleep_pins_mx>;
	pinctrl-names = "default", "sleep";
	phy-mode = "rgmii";
	max-speed = <1000>;
	phy-handle = <&phy0>;
	nvmem-cells = <&ethernet_mac_address>;
	nvmem-cell-names = "mac-address";
 
	mdio0 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "snps,dwmac-mdio";
		phy0: ethernet-phy@6 {
			reg = <6>;
			qca,clk-out-frequency = <125000000>;
 qca,clk-out-strength = <AR803X_STRENGTH_FULL>;
			reset-assert-us = <1000>;
			reset-deassert-us = <2000>; 
			reset-gpios = <&gpiog 0 GPIO_ACTIVE_LOW>;
		};
	};
};

I have added the "eth-ck", because I read somewhere that it would be needed on all cases (it doesn't also work without it). Do I need to enable something else on TF-A or in u-boot?

This topic has been closed for replies.
Best answer by jhi

So finally success!

I have changed the atheros driver to make a phy reset on link notify change (PHY_NOLINK) and do the ar8035_phy_fixup.

13 replies

jhi
jhiAuthor
Senior
January 13, 2022

The u-boot is v2020.10-stm32mp-r2. It doesn't have any of the functions on your patch (your patch is actually removing all the stuff, but I guess it should add those?).

OlivierK
ST Technical Moderator
January 13, 2022

Patch is already present in DV3.1 but you need to apply it if not already done,

for p in `ls -1 ../*.patch`; do patch -p1 < $p; done

indeed the patch is removing the code because reset is handled by the phy driver instead of the ethernet driver.

In drivers/net/dwc_eth_qos.c:

you should have

static struct eqos_ops eqos_stm32_ops = {

...

    .eqos_stop_resets = eqos_null_ops,

    .eqos_start_resets = eqos_null_ops,

...

}

... and reset gpio is handled in /driver/net/eth-phy-uclass.c

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jhi
jhiAuthor
Senior
January 13, 2022

Then I have this patch already.