Skip to main content
Lukas1
Associate II
May 26, 2020
Solved

apt-get: You don't have enough free space

  • May 26, 2020
  • 1 reply
  • 2560 views

Hi,

I installed node.js with apt-get on my STM32MP157C-DK2, which worked great.

Now I want to install another package but it fails

apt-get install nodejs-npm
...
Need to get 7286 kB of archives.
After this operation, 0 B of additional disk space will be used.
E: You don't have enough free space in /var/cache/apt/archives/.

But I think there is still enough free space on the SD Card:

root@stm32mp1:~# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 715M 682M 0 100% /
devtmpfs 150M 0 150M 0% /dev
tmpfs 214M 0 214M 0% /dev/shm
tmpfs 214M 20M 195M 10% /run
tmpfs 214M 0 214M 0% /sys/fs/cgroup
tmpfs 214M 4.0K 214M 1% /tmp
/dev/mmcblk0p4 58M 8.5M 46M 16% /boot
tmpfs 214M 80K 214M 1% /var/volatile
/dev/mmcblk0p7 14G 74M 13G 1% /usr/local
/dev/mmcblk0p5 15M 8.4M 5.1M 63% /vendor

hope someone can help. Otherwise I have to cancel my work with node.js

regards

Lukas

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @Lukas​ 

Your rootfs is full.

Please note in section https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#Limitations

rootfs available space is about 60MB by default. For a better experience it is recommended to flash the Starter Package using the "extensible" flashlayout (*-extensible.tsv).

Extensible flashlayout does not flash userfs partition to extend the rootfs partition to the size of the sdcard.

Olivier

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
May 26, 2020

Hi @Lukas​ 

Your rootfs is full.

Please note in section https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#Limitations

rootfs available space is about 60MB by default. For a better experience it is recommended to flash the Starter Package using the "extensible" flashlayout (*-extensible.tsv).

Extensible flashlayout does not flash userfs partition to extend the rootfs partition to the size of the sdcard.

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lukas1
Lukas1Author
Associate II
May 26, 2020

Hi @Community member​ ,

thanks for your fast reply.

I want to avoid flashing a new image. Is it possible to expand rootfs on the installed image?

Lukas

Fee
Associate II
May 26, 2020

Hi,

you can't resize a mounted partition, as far as I know.

What you can do is take your SD-Card and mount it on a seperate Linux PC. There you can then unmount it and use tools like gparted or fdisk to resize your partition.

Bare in mind, that this is (again as far as I know) just possible if there is no other partition on a higher offset than your rootfs. From your listing i assume that that is the case and the vendor filesystem resides at a higher offset than the rootfs (the rootfs should be on /dev/mmcblk0p6).

If that is the case deleting the vendorfs might help you.