Skip to main content
KSuch.2
Associate II
February 27, 2020
Question

157a-dk1. Hook "update_udev_hwdb" fails.

  • February 27, 2020
  • 2 replies
  • 2004 views

During build with DISTRO=openstlinux-x11 IMAGE=st-example-image-x11 MACHINE=stm32mp1-disco on Ecosystem-1.2 errors arose:

------------------------------------------------------->

ERROR: st-image-vendorfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_udev_hwdb' failed, details in /home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/build-openstlinuxx11-stm32mp1-disco/tmp-glibc/work/stm32mp1_disco-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs

ERROR: st-image-vendorfs-1.0-r0 do_rootfs: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/build-openstlinuxx11-stm32mp1-disco/tmp-glibc/work/stm32mp1_disco-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs.16879

ERROR: Task (/home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb:do_rootfs) failed with exit code '1'

ERROR: st-image-userfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_udev_hwdb' failed, details in /home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/build-openstlinuxx11-stm32mp1-disco/tmp-glibc/work/stm32mp1_disco-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs

ERROR: st-image-userfs-1.0-r0 do_rootfs: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/build-openstlinuxx11-stm32mp1-disco/tmp-glibc/work/stm32mp1_disco-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs.16927

ERROR: Task (/home/support/STM32MP15-Ecosystem-v1.2.0/Distribution-Package/openstlinux-20-02-19/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb:do_rootfs) failed with exit code '1'

---------------------------------------------------------------------->

Must Starter Package be installed before start build?

Log files are attached.

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
February 28, 2020

Hi @KSuch.2​ 

Please confirm you referred to https://wiki.st.com/stm32mpu/wiki/PC_prerequisites and properly install all packages required for Distribution package.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
KSuch.2
KSuch.2Author
Associate II
March 2, 2020

Yes, all prerequisites are fulfilled. But repo init's (or repo sync's) advice to replace /usr/bin/repo is missed. The problem is solved. Suppose to place mention about this advice in step-by-step guide is useful. Thanks.