Skip to main content
DKapu.2
Visitor II
October 12, 2022
Question

Unable to enable PWM driver in uboot

  • October 12, 2022
  • 1 reply
  • 2233 views

We have custom SOM which has been designed with STM32MP157C and we want to enable the backlight of a display panel using a PWM driver in uboot. 

For this, we tried enabling the pwm_backlight.c driver available in /drivers/video/ in uboot.

Following configuration was done to enable the driver:

Changes in the dts file

0693W00000UnvTrQAJ.pngUpdated the Kconfig in /driver/video/

0693W00000UnvJJQAZ.png 

Updated to Makefile in /driver/video/

obj-$(CONFIG_BACKLIGHT_PWM) += pwm_backlight.o

Added the config in defconfig

CONFIG_BACKLIGHT_PWM=y

CONFIG_DM_PWM=y

The image builds successfully, however looking at the log of lists.c during boot, it is unable to find the driver and hence fails to bind.

Another observation is that there is no stm32 core driver file for PWM in uboot. Is this the reason why any of the pwm-based drivers fails to be enabled or is something missing in the configuration mentioned above?

TIA.

This topic has been closed for replies.

1 reply

Associate III
July 17, 2024

Hi, @DKapu.2 .

I am having the same  problem, I  want to configure a  pwm  with  the led_pwm driver, but it's  not working. Did  you manage to make  it work?

 

Regards.