STM32MP157F-DK2 STMCubeProgrammer flashing USB reconnect error
- December 13, 2022
- 3 replies
- 1927 views
While setting up my STM32MP157F-DK2 discovery kit, I followed the steps through the Populate the SDCard section and the flashing process failed with the following message when attempting to flash with the FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv binary.
After failing with the expected flash file I tried flashing again with the FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv binary and the flash process succeeded. Is this expected? I confirmed that my board is a rev F DK-2 and not rev C. I'm not sure what differences there are between the two revisions and if there is any missing functionality with the rev C binary.
16:09:26 : STM32CubeProgrammer API v2.12.0 | Linux-64Bits
16:09:37 : USB speed : High Speed (480MBit/s)
16:09:37 : Manuf. ID : STMicroelectronics
16:09:37 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
16:09:37 : SN : 003F00333438511436383238
16:09:37 : DFU protocol: 1.1
16:09:37 : Board : --
16:09:37 : Device ID : 0x0500
16:10:48 : Read TSV File: /home/loren/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/images/stm32mp1/flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv
16:10:48 : Number of partitions: 13
16:11:45 : Start Embedded Flashing service
16:11:45 : Memory Programming ...
16:11:45 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
16:11:45 : File : tf-a-stm32mp157f-dk2-usb.stm32
16:11:45 : Size : 220.38 KB
16:11:45 : Partition ID : 0x01
16:11:45 : Download in Progress:
16:11:46 : File download complete
16:11:46 : Time elapsed during download operation: 00:00:00.902
16:11:46 : RUNNING Program ...
16:11:46 : PartID: :0x01
16:11:46 : Start operation done successfully at partition 0x01
16:11:46 : Memory Programming ...
16:11:46 : Opening and parsing file: fip-stm32mp157f-dk2-optee.bin
16:11:46 : File : fip-stm32mp157f-dk2-optee.bin
16:11:46 : Size : 1.47 MB
16:11:46 : Partition ID : 0x03
16:11:46 : Download in Progress:
16:11:47 : File download complete
16:11:47 : Time elapsed during download operation: 00:00:01.337
16:11:47 : RUNNING Program ...
16:11:47 : PartID: :0x03
16:11:48 : Reconnecting the device ...
16:11:52 : USB speed : High Speed (480MBit/s)
16:11:52 : Manuf. ID : STMicroelectronics
16:11:52 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
16:11:52 : SN : 003F00333438511436383238
16:11:52 : DFU protocol: 1.1
16:11:52 : Board : --
16:11:52 : Device ID : 0x0500
16:11:52 : Device name : STM32MP157FAC Rev.Z
16:11:52 : Device type :
16:11:52 : Device CPU :
16:11:52 : Start operation done successfully at partition 0x03
16:11:52 : Flashlayout Programming ...
16:11:52 : Running Flashlayout Partition ...
16:11:52 : Reconnecting the device ...
16:11:52 : USB speed : High Speed (480MBit/s)
16:11:52 : Manuf. ID : STMicroelectronics
16:11:52 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
16:11:52 : SN : 003F00333438511436383238
16:11:52 : DFU protocol: 1.1
16:11:52 : Board : --
16:11:52 : Device ID : 0x0500
16:11:52 : Device name : STM32MP157FAC Rev.Z
16:11:52 : Device type :
16:11:52 : Device CPU :
16:11:52 : Flashlayout partition started successfully
16:11:52 : Memory Programming ...
16:11:52 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:52 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:52 : Size : 220.41 KB
16:11:52 : Partition ID : 0x04
16:11:52 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.122
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x04
16:11:53 : Start operation done successfully at partition 0x04
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:53 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:53 : Size : 220.41 KB
16:11:53 : Partition ID : 0x05
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.121
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x05
16:11:53 : Start operation done successfully at partition 0x05
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: metadata.bin
16:11:53 : File : metadata.bin
16:11:53 : Size : 96.00 B
16:11:53 : Partition ID : 0x06
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.006
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x06
16:11:53 : Start operation done successfully at partition 0x06
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: metadata.bin
16:11:53 : File : metadata.bin
16:11:53 : Size : 96.00 B
16:11:53 : Partition ID : 0x07
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.006
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x07
16:11:53 : Start operation done successfully at partition 0x07
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: fip-stm32mp157f-dk2-optee.bin
16:11:53 : File : fip-stm32mp157f-dk2-optee.bin
16:11:53 : Size : 1.47 MB
16:11:53 : Partition ID : 0x08
16:11:53 : Download in Progress:
16:11:54 : File download complete
16:11:54 : Time elapsed during download operation: 00:00:00.788
16:11:54 : RUNNING Program ...
16:11:54 : PartID: :0x08
16:11:54 : Start operation done successfully at partition 0x08
16:11:54 : Memory Programming ...
16:11:54 : Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
16:11:54 : File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
16:11:54 : Size : 64.00 MB
16:11:54 : Partition ID : 0x10
16:11:54 : Download in Progress:
16:11:54 : Error: failed to download Segment[0]
16:11:54 : Error: failed to download the File
16:11:54 : Error: Download partition 0x10 failed
16:11:54 : Error: TSV flashing service failed
16:11:54 : Warning: Connection to device 0x500 is lost
16:11:54 : Disconnected from device.