Skip to main content
Associate
June 5, 2025
Question

Error Encountered While Adding PyQt5 Library into STM32MP13 OpenSTLinux Distribution

  • June 5, 2025
  • 1 reply
  • 1303 views

Hi there, 

I followed the instructions as mentioned below.

  1. repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-6.1-yocto-mickledore-mp1-v24.03.13 (v5.0.3)
  2. repo sync
  3. got pyqt5 files from https://github.com/STMicroelectronics/meta-st-pkgrepo-updates/tree/openstlinux-ecosystem-5.0.0/recipes-python/pyqt5
    and copied them to layers/meta-qt5/recipes-python/pyqt5
  4. run DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh to get the conf/local.conf file

    All packages installed: “Check OK: all required packages are installed on host.”
  5. added IMAGE_INSTALL:append = " python3-pyqt5" to my image in build-openstlinuxweston-stm32mp1/conf/local.conf
  6. bitbake st-weston image

 

However, I'm encountering the following error:

ERROR: Task (/home/abcd/DistributionPackage/layers/meta-openembedded/meta-oe/recipes-support/libiio/libiio_git.bb:do_configure) failed with exit code '1'

 

when i checked error log in that it was mentioned  #include<pthread.h> compilation terminated. But that header was included in sysroot.

Could you please help me resolve this?

 

1 reply

PPAGE.13
ST Employee
July 29, 2025

Hi,

I would recommend moving to Qt6 and PySide6, you will get a more recent package.

You can get PySide6 recipe here:

https://layers.openembedded.org/layerindex/recipe/380679/

There is a dependency on meta-clang.

 

For Qt6 support on MP1 or MP2, please refer to following documentation:

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Distribution_Package

 

BR,

Philippe.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.