2025-04-25 6:45 AM
Hello! I have succesfully run some test using the model zoo services repo. For classification and object detection I understand. What I cannot find out is whether it is possible to make a custom inference script. My use case requires to run an object detection and then do binary classification on the cropped objects using a classification model. Is it possible to write such a custom script using models generated from the zoo? Also, can i run inference without a camera on images or video? I have purchased the STM32MP257F-EV1 board.Thanks in advance!