Skip to main content
SLetter
Associate III
October 6, 2022
Question

We are building a board based on ST32mp157c and have problems enabling USB port 1. We did not include the ECMF02-2AMX6 choke. Could this be the problem?

  • October 6, 2022
  • 6 replies
  • 3285 views

We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power., Otherwise we are using the basic defconfig and the DK2 devtree.

This topic has been closed for replies.

6 replies

Kevin HUBER
ST Employee
October 10, 2022

Hello @nonesuchetter​ ,

ECMF02-2AMX6 is used to protect from ESD and EMI, it should work without it.

What is the problem that you encounter with the USB port 1? Do you have an error?

The port related to OTG is the port 2:

https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration#DT_bindings_documentation

Can you explain the modifications that you made, because you normally doesn't need to modify code part:

We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power.,

May I know which Ecosystem are you using and please can you indicate the file that you are using when you say "using the basic defconfig" ?

To help you, I will also need the traces made during the boot by your board.

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SLetter
SLetterAuthor
Associate III
October 11, 2022
Steve Letter You're never to old to learn something stupid.  -- unknown
SLetter
SLetterAuthor
Associate III
October 12, 2022

For some reason my answer didn't come through. I include it here.

What is the problem that you encounter with the USB port 1? Do you have an error?

The port doesn't reset.

The port related to OTG is the port 2:

https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration#DT_bindings_documentation

Can you explain the modifications that you made, because you normally doesn't need to modify code part:

Commented out board_check_usb_power();

in board/st/stm32mp1/stm32mp1.c

We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power.,

May I know which Ecosystem are you using and please can you indicate the file that you are using when you say "using the basic defconfig" ?

Ecosystem-v3.1.0 Build u-boot as follows:

make stm32mp15_basic_defconfig

make menuconfig (to enable debug log)

make -DEVICE_TREE=stm32mp157c-dk2 all

To help you, I will also need the traces made during the boot by your board.

I have attached the u-boot startup log as well as the usb start log. Attached to the USB A (dm1, dp1) port is a full speed device, a ZIP 250 drive.

SLetter
SLetterAuthor
Associate III
October 12, 2022

Second attached file

Olivier GALLIEN
ST Technical Moderator
October 28, 2022

Hi @nonesuchetter​ ,

Are you aware that ST does not recommend and support product using basic_defconfig ?

It's remains present on 3.1 ecosystem as a legacy to build the U-Boot SPL flavor require for DDR test and tuning.

In link below it's stated that Uboot-SPL has a very limited feature set

https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Boot_chains_overview#Boot_chains_features_set

Maybe you are fully aware and already handle this, but anyway, ST cannot support you really further in this direction.

Any rational to not use trusted config?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SLetter
SLetterAuthor
Associate III
October 29, 2022
We have this issue with both builds, basic and trusted. We will be using trusted configuration in our product, support for this along with the crypto engine was a deciding factor going with this SOC (we provide security devices for the military).
Steve Letter
Sent from my Symbolics Lisp Machine using zmail.