Associate II
November 5, 2019
Solved
Toogle Pins for STM32MP157C-DK2
- November 5, 2019
- 12 replies
- 5987 views
Hello,
I am working on the evaluation board STM32MP157CDk2
I am trying to add my code in the main method while loop in order to toogle pins.
I added the following code:
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(atoi(1), GPIO_PIN_11);
HAL_Delay(100);
HAL_GPIO_TogglePin(atoi(0), GPIO_PIN_11);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */I have two questions.
1) I get the following error (attached) after i choose target and then program chip
2) I am connected through usb and UART in the eclipe, am using the system work bench as an IDE. Is there something to do before doing the build for connecting with the device in a special way?. I can see in the console that i am connected to the board. and Eclipse shows the message at the buttom (Serial Console in use).
I am new to this. I appreciate your help alot
Best Regards