Skip to main content
dimtass
Associate II
September 8, 2020
Solved

Mistake in STM32MP1-DK2 schematics?

  • September 8, 2020
  • 1 reply
  • 1128 views

Hi all.

The en.MB1272-DK2-C01_Schematic.pdf states that

ARD_A0 : PF14 -> ADC1_IN0

ARD_A1 : PF13 -> ADC1_IN1

ARD_A2 : ANA0 -> ADC2_IN6

ARD_A3 : ANA1 -> ADC2_IN2

I've spend quite some time to figure out that this is wrong and the correct pinout is:

ARD_A0 : PF14 -> ADC2_IN6

ARD_A1 : PF13 -> ADC2_IN2

ARD_A2 : ANA0 -> ADC1_IN0

ARD_A3 : ANA1 -> ADC1_IN1

Can you please verify and if it's so then update the pdf?

Regards.

This topic has been closed for replies.
Best answer by PatrickF

Hello,

I confirm the discrepancies (which are also present on UM2534).

Update of documents will occur, but not in very short term.

1 reply

PatrickF
PatrickFBest answer
ST Employee
September 9, 2020

Hello,

I confirm the discrepancies (which are also present on UM2534).

Update of documents will occur, but not in very short term.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent