Solved
I want to power the STM32MP157 card by the + 5V of the CN2 connector to integrate the card on a motherboard of a control system. The card does not boot if power is supplied from CN2.
Only the power supply via USB C CN6 allows booting with detection of the presence of voltage on GPIO PA5 and PA4. Is there a way to modify this control mode and be able to boot with a CN2 power supply? Is it possible to modify the FW so as not to read the two GPIOs ? Thank for help.