How to use STM32U5 with FreeRTOS™ in tickless mode
- Oct 28, 2026 6:55 PM UTC
- 1 reply
- 8781 views
Introduction
In this article, we cover the needed steps to use the FreeRTOS™ in tickless mode, specifically entering in STOP2 low-power mode with the STM32U5. In this example, we use the X-CUBE-FREERTOS™ pack with the LPUART and EXTI as the wake up sources.
All the implementation was done over STM32CubeIDE 1.12.1 with STM32CubeMX 6.8.1, STM32CubeU5 1.2.0, and X-CUBE-FREERTOS 1.0.1. The NUCLEO-U575ZI-Q with STM32U575ZIT6Q MCU hardware was used but the steps can be easily tailored to any other ST microcontroller, with minor changes.
Development
First, create a project in STM32CubeMX for the target microcontroller (MCU). In this case, create the project for STM32U575ZIT6Q. In STM32CubeMX, select "STM32U575ZIT6Q," and then click "Start Project."

When this popup appears, create a project with TrustZone disabled.

After its creation and naming, open the SYS tab. Under System Core, selecta timer as Timebase Source, TIM6 was arbitrarily selected. This step is needed since the SysTick timer is used by FreeRTOS™.

While in the System Core, locate the GPIO tab and set the PC13 as EXTI with External Interrupt Mode with Rising edge trigger detection. There is a push-button (active high) connected into this pin in NUCLEO-U575ZI-Q with a pull-down and a hardware debounce filter.

Under Connectivity tab, enable the LPUART1 as Asynchronous mode and apply your settings. In this tutorial, we use the standard UART settings (8/N/1), but with the 9600 bits/s for the baud rate.

Back to the System Core tab, open the NVIC and enable both EXTI Line 13 and LPUART global interrupts.


Change the Power Regulator to SMPS under PWR -> Power saving mode to achieve better current consumption values in low-power.







Once opened the project, open the Core/Src/app_freertos.c file. All the code implementations are done in this file. The first code is to include the stdio to use the printf function to log through the LPUART.
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes *//* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN Variables */
__IO uint8_t rxChar;
extern UART_HandleTypeDef hlpuart1;
/* USER CODE END Variables */ /* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN FunctionPrototypes */
extern void SystemClock_Config(void);
/* USER CODE END FunctionPrototypes */void MX_FREERTOS_Init(void) {
/* USER CODE BEGIN Init */
__HAL_RCC_LPUART1_CLKAM_ENABLE(); //Enable LPUART in Autonomous mode
HAL_UARTEx_EnableStopMode(&hlpuart1); //Retain the LPUART clock in STOP
HAL_UART_Receive_IT(&hlpuart1, (uint8_t*)&rxChar, 1);
/* USER CODE END Init */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
osSemaphoreAcquire(WakeSemHandle, osWaitForever);
/* USER CODE END RTOS_SEMAPHORES *
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
/* USER CODE BEGIN defaultTask */
/* Local variables */
printf("Default task started...\r\n");
/* Infinite loop */
for(;;)
{
printf("Default task waiting for a semaphore...\r\n");
osSemaphoreAcquire(WakeSemHandle, osWaitForever);
printf("Default task running...\r\n");
HAL_Delay(300);
}
/* USER CODE END defaultTask */
}/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
int __io_putchar(int ch)
{
HAL_UART_Transmit(&hlpuart1, (uint8_t *)&ch, 1, 10);
return ch;
}
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
printf("Woke-up from EXTI\r\n");
osSemaphoreRelease(WakeSemHandle);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
printf("Woke-up from LPUART, message: %c\r\n", rxChar);
HAL_UART_Receive_IT(&hlpuart1, (uint8_t*)&rxChar, 1);
osSemaphoreRelease(WakeSemHandle);
}
/* USER CODE END Application *//* USER CODE BEGIN PREPOSTSLEEP */
__weak void PreSleepProcessing(uint32_t ulExpectedIdleTime)
{
/* place for user code */
HAL_SuspendTick();
SysTick->CTRL &= ~SysTick_CTRL_TICKINT_Msk;
printf("Entering in STOP2 Mode...\r\n");
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
}
__weak void PostSleepProcessing(uint32_t ulExpectedIdleTime)
{
/* place for user code */
SystemClock_Config();
SysTick->CTRL |= SysTick_CTRL_TICKINT_Msk;
printf("\nExit from STOP2 Mode\r\n");
HAL_ResumeTick();
}
/* USER CODE END PREPOSTSLEEP */We are all set! Compile and program the code into MCU. Perform a power-cycle to disable the Debugger to avoid unexpected Wake-up sources and elevated power consumption. Connect the UART into a Terminal and see the results!
NOTE2: The LPUART1 is not the default connection to the ST-LINK VCOM embedded in NUCLEO-U575ZI-Q. You should connect this manually to a computer or change the solder bridges as illustrated in this image, extracted from the board’s user manual:

Results
When the application starts, the DefaultTask is started and runs until the osSemaphoreGet instruction. After that, the Idle task is started and the PreSleepProcessing function is called and the MCU can enter in Low-Power Tickless mode.As set in the project, there are 2 available wake-up interrupt sources. The LPUART1 that waits for a character to be received and the EXTI that waits for the button to be pressed. Whenever an interruption happens, the PostSleepProcessing function is called, where we have the code to prepare the MCU after waking up from STOP2 mode.
The interrupt calls the callback function (according to the wake up source used) which releases a semaphore, letting the DefaultTask back to run mode until the osSemaphoreGet instruction is detected again.
The expected application behavior is illustrated in the image below, showing the TeraTerm view and messages output:


To offer a quick comparison between the consumption of LSE and HSI as clock sources for the LPUART, the following graph displays the application consumption while utilizing the HSI.

Conclusion
This article demonstrates that the FreeRTOS Tickless mode is a valuable feature when low-power profiles are needed while using RTOS. As demonstrated in the tutorial, the process is straightforward, which the RTOS automatically manages the moment the kernel enters in Idle mode. This allows us to invoke and select the low power mode from the MCU desired, in this case, the STOP2.That concludes our tutorial! We hope that you enjoyed reading it.
Useful links:
Here are some links that were used to build this application and could be useful for your developments related to the X-CUBE-FREERTOS and STM32U5.
NUCLEO-U575ZI-Q - STM32 Nucleo-144 development board with STM32U575ZIT6Q MCU, SMPS, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics
STM32U575ZI - Ultra-low-power with FPU Arm Cortex-M33 MCU with TrustZone, 160 MHz with 2 Mbytes of Flash memory - STMicroelectronics
X-CUBE-FREERTOS - FreeRTOS software expansion for STM32Cube - STMicroelectronics
STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
STM32CubeMonPwr - Graphical tool displaying on PC power data coming from STLink-V3PWR - STMicroelectronics
edited by