Skip to main content
ST AME Support NF
ST Employee
November 16, 2021

How to create an I2C target device using the STM32Cube Library

  • November 16, 2021
  • 6 replies
  • 60996 views

Introduction

In this article we will see how to create an I2C target device with interrupts using the STM32CubeMX and STM32Cube HAL Library. All the I2C target communication will be handled by firmware.
 

1. Pre-requisites

1.1 Hardware:

  • Micro USB cable: to power and program the board
  • Nucleo-G070RB board

1795.png
 

1.2 Software

  • STM32CubeIDE

 

3. Theory


Adding an I2C target to an application can be a bit tricky due to the complexity of the I2C protocol. In this article we will show you how to add asynchronous I2C target code using the STM32cubeIDE tool for I2C configuration and then include the necessary code to handle the I2C target asynchronous mode using interrupts. For this article, a Total Phase Aardvark is used as the I2C controller.
1796.png
The pinout of the Aardvark:
1797.png
Nucleo-G070RB:

  • PA9 and PA10 of the STM32G070 on the Nucleo-G070RB will be used for the I2C communication.


1798.png
Connections:

  • NUCLEO-G070RB Set-up:
    • Connect the SCL  line of Master Aardvark to I2C_SDA line of the Nucleo target Board (PA9: pin 21 of CN10).
    • Connect the SDA line of Master Aardvark to I2C_SDA line of the Nucleo target Board (PA10: pin 33 of CN10).
    • Connect GND of Aardvark board to GND of Nucleo Board.


The software Control Center from Total Phase will be used to setup and control the master I2C communications with the STM32 I2C target code.
 

 4. Steps

 

  1. Open STM32CubeIDE
  2. Create a new project using the NUCLEO-G070RB board


1799.png
 

  1. Enter a name for the project (in this case, the project is named I2CSlave).

1800.png
 

  1. Board Project Options:
    • Initialize all peripherals with their default settings by clicking on Yes when this dialog window appears:


1801.png

  1. Select the I2C peripheral
  • In Pinout & Configuration Tab, under Communication, click on I2C1 peripheral.


1802.png
 

  1. Enable I2C mode and keep the default Timing Configuration

1803.png
 

  1. Configure the target part by adding the I2C slave address
  • For this example, 0x20 will be used as the I2C slave address. The rest of the default configuration is kept.

1804.png
 

  1. Enable I2C1 interrupts
  • As mentioned earlier, the I2C communications will be handled using Interrupts which is the most convenient and efficient way to handle target communication.
  • In NVIC tab enable the Interrupts as shown below:

1805.png

 5. Code generation

  1. Generate Code
  • Saving the project generates the code
  1. Add code:
  • Now that the I2C peripheral is configured using the STM32CubeIDE, now add some code to handle the I2C target communication for both Transmit and Receive operations.
  • In main.c, add the following code at the beginning of the file:
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define COUNTOF(__BUFFER__) (sizeof(__BUFFER__) / sizeof(*(__BUFFER__)))
/* Size of Transmission buffer */
#define TXBUFFERSIZE (COUNTOF(aTxBuffer))
/* Size of Reception buffer */
#define RXBUFFERSIZE TXBUFFERSIZE
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
__IO uint32_t Transfer_Direction = 0;
__IO uint32_t Xfer_Complete = 0;
/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* Buffer used for transmission */
uint8_t aTxBuffer[4];

/* Buffer used for reception */
uint8_t aRxBuffer[4];
/* USER CODE END PD */
  • Add following code in the main function which initializes the receive and transmit buffers being used.

 

 /* USER CODE BEGIN Init */
 aRxBuffer[0]=0x00;
 aRxBuffer[1]=0x00;
 aRxBuffer[2]=0x00;
 aRxBuffer[3]=0x00;
 aTxBuffer[0]=0xAA;
 aTxBuffer[1]=0xBB;
 aTxBuffer[2]=0xCC;
 aTxBuffer[3]=0xDD;
 /* USER CODE END Init */
…
  • Enable the Listen mode with Interrupts for the I2C: The Listen Mode will wait for an I2C Event to occur and will be treated in the Interrupt Service Routine of the I2C.
/* USER CODE BEGIN 2 */
 if(HAL_I2C_EnableListen_IT(&hi2c1) != HAL_OK)
 {
 /* Transfer error in reception process */
 Error_Handler();
 }
 /* USER CODE END 2 */
  • Xfer_Complete variable will be updated in the call back function that will be added later. Basically, once a target receive or transmit transaction is completed, the Listen mode Interrupt will be entered again.
/* USER CODE BEGIN WHILE */
 while (1)
 {

 if (Xfer_Complete ==1)
 {
 HAL_Delay(1);
 /*##- Put I2C peripheral in listen mode process ###########################*/
 if(HAL_I2C_EnableListen_IT(&hi2c1) != HAL_OK)
 {
 /* Transfer error in reception process */
 Error_Handler();
 }
 Xfer_Complete =0;
 }

 /* USER CODE END WHILE */

…



In these functions, the call back functions are added and manage the slave transmit or slave receive part of the code.
 
/* USER CODE BEGIN 4 */
/**
 * @brief Tx Transfer completed callback.
 * I2cHandle: I2C handle.
 * @note This example shows a simple way to report end of IT Tx transfer, and
 * you can add your own implementation.
 * @retval None
 */

void HAL_I2C_SlaveTxCpltCallback(I2C_HandleTypeDef *I2cHandle)
{
 /* Toggle LED4: Transfer in transmission process is correct */

 Xfer_Complete = 1;
 aTxBuffer[0]++;
 aTxBuffer[1]++;
 aTxBuffer[2]++;
 aTxBuffer[3]++;

}


/**
 * @brief Rx Transfer completed callback.
 * I2cHandle: I2C handle
 * @note This example shows a simple way to report end of IT Rx transfer, and
 * you can add your own implementation.
 * @retval None
 */
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *I2cHandle)
{
 /* Toggle LED4: Transfer in reception process is correct */

 Xfer_Complete = 1;
 aRxBuffer[0]=0x00;
 aRxBuffer[1]=0x00;
 aRxBuffer[2]=0x00;
 aRxBuffer[3]=0x00;
}



/**
 * @brief Slave Address Match callback.
 * hi2c Pointer to a I2C_HandleTypeDef structure that contains
 * the configuration information for the specified I2C.
 * TransferDirection: Master request Transfer Direction (Write/Read), value of @ref I2C_XferOptions_definition
 * AddrMatchCode: Address Match Code
 * @retval None
 */
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
 Transfer_Direction = TransferDirection;
 if (Transfer_Direction != 0)
 {
 /*##- Start the transmission process #####################################*/
 /* While the I2C in reception process, user can transmit data through
 "aTxBuffer" buffer */
 if (HAL_I2C_Slave_Seq_Transmit_IT(&hi2c1, (uint8_t *)aTxBuffer, TXBUFFERSIZE, I2C_FIRST_AND_LAST_FRAME) != HAL_OK)

 {
 /* Transfer error in transmission process */
 Error_Handler();
 }

 }
 else
 {

 /*##- Put I2C peripheral in reception process ###########################*/
 if (HAL_I2C_Slave_Seq_Receive_IT(&hi2c1, (uint8_t *)aRxBuffer, RXBUFFERSIZE, I2C_FIRST_AND_LAST_FRAME) != HAL_OK)
 {
 /* Transfer error in reception process */
 Error_Handler();
 }

 }

}

/**
 * @brief Listen Complete callback.
 * hi2c Pointer to a I2C_HandleTypeDef structure that contains
 * the configuration information for the specified I2C.
 * @retval None
 */
void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef *hi2c)
{
}

/**
 * @brief I2C error callbacks.
 * I2cHandle: I2C handle
 * @note This example shows a simple way to report transfer error, and you can
 * add your own implementation.
 * @retval None
 */
void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *I2cHandle)
{
 /** Error_Handler() function is called when error occurs.
 * 1- When Slave doesn't acknowledge its address, Master restarts communication.
 * 2- When Master doesn't acknowledge the last data transferred, Slave doesn't care in this example.
 */
 if (HAL_I2C_GetError(I2cHandle) != HAL_I2C_ERROR_AF)
 {
 Error_Handler();
 }
}
/* USER CODE END 4 */​

 

 6. Project Build


Build the project, enter debug mode and run the code
1806.png
  • Enter Debug session: this programs the code into the flash and then starts the debug session
1807.png
  • Then click on the Resume icon which will execute the code.
1808.png
In the Total Phase Control Center software, connect to the Aardvark device. The Aardvark is configured to act as an I2C Master. We are testing our code for I2C target transmit and receive by sending some I2C Master Reads and Writes as follows:
  • Send a buffer of 4 bytes “01 02 03 04” two times (Master Write).
  • Master read of 4 bytes three times (Master Read).
1809.png
As shown in the Transaction Log, the STM32G0 I2C target code received and transmitted data as expected.

7. Related links

STM32G070RB - Datasheet
STM32G0x0 advanced Arm®-based 32-bit MCUs - Reference manual
STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
NUCLEO-G070RB - STM32 Nucleo-64 development board with STM32G070RB MCU, supports Arduino and ST morpho connectivity - STMicroelectronics
Aardvark I2C/SPI Host Adapter - Total Phase
Total Phase Control Center
This topic has been closed for replies.

6 replies

SMali.4
Associate
June 29, 2022

Hello, I am woking on STM32G030F6P6 microcontroller.

I am trying to receive data from master using above code (STM32G030F6P6 in slave mode)

HAL_I2C_Slave_Seq_Transmit_IT function is working properly.

But HAL_I2C_Slave_Seq_Receive_IT function not receiving data ( ie. not updating aRxBuffer ) ( program goes into HAL_I2C_AddrCallback routine)

Can some please help with this problem?

Rpatt.1
Visitor II
August 12, 2022

I was having the same issue as SMali.4 where it seemed like aRxBuffer was not receiving any data. I was trying to debug print the data in HAL_I2C_AddrCallback(). But I found that it does work correctly if I print the contents of aRxBuffer in HAL_I2C_SlaveRxCpltCallback() instead.

PTara.2
Visitor II
October 3, 2022

I had an issue that sequential call to i2cdetect -y 1 made I2C SCL line remain low.

This is because HAL_I2C_AddrCallback does not reset Xfer_Complete variable, so main function goes to infinite loop without listening for I2C events.

Issue fixed adding Xfer_Complete = 1; at the end of HAL_I2C_AddrCallback

JAlbe.4
Visitor II
February 14, 2023

The Example didn't work properly on my device. After many hours of debugging I found the solution. The Code which is stored within the HAL_I2C_AddrCallback have to be within the main to prevent timing errors.

Within the Private defines I create two "unit_8" which are used as boolean within the following code:

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* Buffer used for transmission */
uint8_t aTxBuffer[3];
 
/* Buffer used for reception */
uint8_t aRxBuffer[1];
uint8_t getMasterInput = 0;
uint8_t getTransferDirection = 0;
/* USER CODE END PD */

Within the Main my Code is:

	/* USER CODE BEGIN WHILE */
	while (1) {
		if (getMasterInput == 1) {
			getMasterInput = 0;
			if (getTransferDirection == 0) {
 
				if (HAL_I2C_Slave_Seq_Transmit_IT(&hi2c1, (uint8_t*) aTxBuffer,
						TXBUFFERSIZE, I2C_NEXT_FRAME) != HAL_OK)
				//if (HAL_I2C_Slave_Transmit(&hi2c1, (uint8_t *)aRxBuffer, TXBUFFERSIZE) != HAL_OK)
				// if (HAL_OK != HAL_OK)
						{
 
					Error_Handler();
				}
 
			} else {
 
				if (HAL_I2C_Slave_Seq_Receive_IT(&hi2c1, (uint8_t*) aRxBuffer,
						RXBUFFERSIZE, I2C_NEXT_FRAME) != HAL_OK)
				//if (HAL_OK != HAL_OK)
						{
 
					Error_Handler();
				} else {
					HAL_Delay(1 * RXBUFFERSIZE);
				}
 
			}
			GPIOG->BSRR = DBG_PIN_Pin;
		}
 
		HAL_GPIO_WritePin(GPIOG, DBG_PIN_Pin, GPIO_PIN_RESET);
 
		if (Xfer_Complete == 1) {
			// HAL_Delay(1);
			/*##- Put I2C peripheral in listen mode proces ###########################*/
			if (HAL_I2C_EnableListen_IT(&hi2c1) != HAL_OK) {
				/* Transfer error in reception process */
				Error_Handler();
			}
			Xfer_Complete = 0;
		}
 
		/* USER CODE END WHILE */

Therefor my HAL_I2C_AddrCallback function looks like that:

void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection,
		uint16_t AddrMatchCode) {
	getMasterInput = 1;
	getTransferDirection = TransferDirection;
}

With this changes to the Example from ST my device works properly fine.

TFesa.1
Associate II
March 28, 2023

Hello Laura, thanks for your comment.

I'm trying to connect an STM32 as a slave in I2C to an RPI.

So I tried to follow the given documentation. When I apply your modifications, I get several errors.

First of all, TransferDirection is not recognized if I put it in the main. It was originally in HAL_I2C_AddrCallback. I didn't quite understand if you were moving the whole function or just its contents. 

If it's just the content, then you replace the HAL_I2C_AddrCallback function with the one you propose below after copying the first content into main, is that right? 

Then, as for your second piece of code, you say what is in my main is: ...

Do you add that to main, replace it, or put it in /* USER CODE BEGIN WHILE */ instead? 

For me, putting it in /* USER CODE BEGIN WHILE */ I get errors for GPIOG->BSRR = DBG_PIN_Pin; with DBG_PIN_Pin and GPIOG not declared. 

I thank you a lot in advance for the time you can give me

Thomas

ORam.1
Visitor II
April 26, 2023

Hello.

Can some one send the full Master code to communicate with the slave ??

Thanks ram