Skip to main content
TAlli.1
Visitor II
February 14, 2023
Solved

what is the max soldering temperature for STM32-WB55RG?

  • February 14, 2023
  • 1 reply
  • 1557 views

..

This topic has been closed for replies.
Best answer by KDJEM.1

Hello @TAlli.1​ and welcome to Community :) ,

The max soldering temperature dependent for package.

So, if you have WLCSP package, you can refer to TN1163 and precisely PCB assembly guidelines section.

For all other package, you can refer to AN2639 table 3 and to the standard soldering JEDEC J-STD-020.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you.

Kaouthar

1 reply

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
February 28, 2023

Hello @TAlli.1​ and welcome to Community :) ,

The max soldering temperature dependent for package.

So, if you have WLCSP package, you can refer to TN1163 and precisely PCB assembly guidelines section.

For all other package, you can refer to AN2639 table 3 and to the standard soldering JEDEC J-STD-020.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.