Skip to main content
VSaro.1
Associate
August 4, 2022
Question

unexpected interrupt when running the example FLASH_EraseProgram for NUCLEOWB15

  • August 4, 2022
  • 5 replies
  • 1569 views

Hi,

I need to write some config data to the flash and tried to start from the example FLASH_EraseProgram for NUCLEOWB15. But I got problems already when running the example without any modification. My setup:

  • NUCLEO-WB15CC board
  • FLASH_EraseProgram without modifications
  • STM32CubeIDE Version: 1.10.1 Build: 12716_20220707_0928 (UTC)
  • Import STM32 Cube Example->Board NUCLEO-WB15CC->FLASH_EraseProgram
  • build, and DEBUG FLASH_EraseProgram
  • and the debugger ends in the Default Handler Infinite Loop

Wen I look at the registers, the program counter shows WWDG_IRQHandler, maybe a watchdog problem?

Any help is appreciated!

Regards Volker

Content of the registers:

General Registers      General Purpose and FPU Register Group   

   r0   56      

   r1   536871108      

   r2   1476411392      

   r3   1073807810      

   r4   536871068      

   r5   0      

   r6   0      

   r7   536883164      

   r8   0      

   r9   0      

   r10   0      

   r11   0      

   r12   0      

   sp   0x20002fb8      

   lr   -7      

   pc   0x80001ec <WWDG_IRQHandler>      

   xpsr   16777219      

   d0   0      

   d1   0      

   d2   0      

   d3   0      

   d4   0      

   d5   0      

   d6   0      

   d7   0      

   d8   0      

   d9   0      

   d10   0      

   d11   0      

   d12   0      

   d13   0      

   d14   0      

   d15   0      

   fpscr   0      

   primask   0      

   basepri   0      

   faultmask   0      

   control   0      

   msp   0x20002fb8      

   psp   0x0      

   s0   0      

   s1   0      

   s2   0      

   s3   0      

   s4   0      

   s5   0      

   s6   0      

   s7   0      

   s8   0      

   s9   0      

   s10   0      

   s11   0      

   s12   0      

   s13   0      

   s14   0      

   s15   0      

   s16   0      

   s17   0      

   s18   0      

   s19   0      

   s20   0      

   s21   0      

   s22   0      

   s23   0      

   s24   0      

   s25   0      

   s26   0      

   s27   0      

   s28   0      

   s29   0      

   s30   0      

   s31   0      

This topic has been closed for replies.

5 replies

VSaro.1
VSaro.1Author
Associate
August 4, 2022

I tested other examples, just to see if there is a pattern:

- FLASH_WriteProtection same problem

- WWDG_Example works

- WWDG_RefreshUntilUserEvent_Init works

- GPIO_IOToggle works

- EXTI_ToggleLedOnIT_Init works

- BSP_Example works

VSaro.1
VSaro.1Author
Associate
August 4, 2022

Investigating further I found a difference of FLASH_EraseProgram to WWDG_Example in the NVIC settings. I added "Generate IRQ handler" accordingly and now the program ends in the HardFault_Handler instead of the Default-handler:0693W00000QMxyXQAT.png0693W00000QMy0JQAT.png

Semer CHERNI
ST Employee
August 16, 2022

Hello @VSaro.1​ 

First thanks for posting.

In this case I recommend that you check the user configuration under the Option Bytes for your SOC with CubeProgrammer.

Specifically the IDWGSW it should be Unchecked.

0693W00000QNnwOQAT.png 

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VSaro.1
VSaro.1Author
Associate
August 29, 2022

Thanks Semer, it seems to work now.

Kind regards

Volker

VSaro.1
VSaro.1Author
Associate
August 29, 2022

Hello Semer,

ok, after unchecking IDWGSW it doesn't end in the WWDG_IRQHandler() but...

the program never returns from the call to HAL_FLASHEx_Erase(&EraseInitStruct, &PageError), see line 145 in FLASH_EraseProgram/Src/main.c.

Is there another option maybe?

Kind regards

Volker