Skip to main content
KKIM.6
Senior
March 12, 2024
Question

Unable to start FUS. FUS version is 0.0.0.0 and FUS_STATE_ERR_UNKNOWN

I'm trying to fix a P-Nucleo-WB55 board using CubeProgrammer.

However, the board shows a 0.0.0.0 version of FUS and Stack and I cannot start FUS.

I don't know why there is no version because the FUS cannot be deleted forever in the FUS upgrade document.

So, How can I update FUS in this version?

The SBRV option byte is 0x3ffff is it common?

KKIM6_0-1710278560335.png

KKIM6_1-1710278589868.png

KKIM6_2-1710278620227.png

 

 

This topic has been closed for replies.

6 replies

STTwo-32
ST Technical Moderator
March 13, 2024

Hello @KKIM.6 

According to the SBRV value, FUS is not running. I suggest you try to update your firmware Following this wiki and using the last version (included in the version 1.18.0 of the STM32CubeWB).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KKIM.6
KKIM.6Author
Senior
March 13, 2024

Could you send the link again?

 

I'm trying to upgrade FUS following the "STM32WB Firmware Upgrade Service wiki" but there is no description when FUS does not exist.

 

Remi QUINTIN
ST Technical Moderator
April 12, 2024

The SBRV value is pointing on the safeboot which means something went badly wrong during the update.

I assume the SFSA value to be FFFF protecting the last sector.

Did you already program this board? 

I would be nice to get the ESE and SFSA values.

 

Then one thing that may work to recover your board in a manufactory state is to write the value 0x00008000 at the address 0x5800040C. This should work if ESE option byte is checked.

 

Visitor II
February 24, 2025

Hello,

I encountered a similar issue where the FUS became unresponsive after sending an event signal. STM32CubeProgrammer now reports the FUS and wireless stack versions as v0.0.0.0.

I am unsure what caused this issue. Multiple recovery attempts, including updating the FUS firmware, did not work.

Were you able to fix the issue? How can I avoid this in the future? Any guidance would be appreciated.

Thanks!

Lubos KOUDELKA
ST Employee
February 25, 2025

Step by step guidance for restoring option bytes corruption as defined in AN5185, page 10.

  • Connect MCU using Stlink USB and start STM32CubeProgrammer
  • If there is problem to connect using STM32CubeProgrammer, add jumper to BOOT0 pin

1.set RDP AA (will remove the PCROP as well)

  • Ensure PCROP and RDP is not active

2.set OB to boot in System Flash (nBoot0 = 0)

3.reboot

4.connect STM32CubeProgrammer with hotplug

5.start CPU2 using write 0x00008000 at 0x5800040C