Skip to main content
Associate III
July 22, 2024
Solved

STM32WBA55G-DK1 not compatible with all mobiles

  • July 22, 2024
  • 3 replies
  • 1385 views

Hi 
I recently purchased DK board and connected to the phone to check the dumped code.
But, I couldn't listen to any music nor call. 

I realised only few selected mobiles with BLE Audio can be used to test the board.
Any solution to this? 
@STTwo-32 @KDJEM.1 
Thanks in advance!

This topic has been closed for replies.
Best answer by Pallavi

Hi @Andrew Neil 

Thank you. Got it!
I have understood that only few mobiles with BLE feature can be used to test the Audio features as mentioned in

https://wiki.st.com/stm32mcu/wiki/Connectivity:Bluetooth_LE_Audio_-_STM32WBA_Telephony_%26_Media_Audio_Profile

3 replies

Andrew Neil
Super User
July 22, 2024

@STTwo-32  has already  answered this question for you:

https://community.st.com/t5/stm32-mcus-wireless/classic-bluetooth-in-stm32wba55/m-p/694969

 

See also: https://community.st.com/t5/stm32-mcus-wireless/audio-on-stm32wb55cg/m-p/694244/highlight/true#M20065 

 

The ST Chips do BLE only; they do not do "Classic" Bluetooth - so you obviously won't be able to use them with phones which only have classic Bluetooth!

 


@Pallavi wrote:

Any solution to this? 


You will need a separate Classic BT module to support Classic BT.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PallaviAuthorBest answer
Associate III
July 23, 2024

Hi @Andrew Neil 

Thank you. Got it!
I have understood that only few mobiles with BLE feature can be used to test the Audio features as mentioned in

https://wiki.st.com/stm32mcu/wiki/Connectivity:Bluetooth_LE_Audio_-_STM32WBA_Telephony_%26_Media_Audio_Profile

Andrew Neil
Super User
July 23, 2024

Yes, Auracast (LE Audio) is a very new BLE feature (only released this year?) - so very few phones yet support it.

Please mark the solution.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.