Skip to main content
Associate III
Jul 19, 2024 5:14 AM UTC
Question

STM32WBA52CGU6 Advertisement Issue: Discoverable in iOS/Windows not in Android

Hi Concerned Team,

Need valuable support:
1. Advertisement Issue: Discoverable in iOS/Windows not in Android
- Board: NUCLEO-STM32WBA52
- MCU: STM32WBA52CGUX
- SDK: 1.14.0
- Due to unavailability of out of box any BLE example code for STM32WBA52 series,
  Used base code for STM32WBA55 series and converted firmware for STM32WBA52,
  Tried examples: peer_to_peer_server_ota, heartrate_ota and beacon.
- Found strange case for all three examples that:
  Device advertisement found in iOS(BLE5.3) and Windows(BLE5.0), with good RSSI around -26dBm to -34dBm,
  even able to connect, read, write and notify perfectly,
  But device advertisement not found in Android phones:
  MI-11X(Android-V13, BLE5.1), Nokia-G42-5G(Android-V13, BLE5.1)
- peer_to_peer_sever_ota (STM32CubeIDE) advertisement found in windows and iOS related screenshots attached here.
fa097269-708d-4026-8346-30d40f165533.jpgRef: Windows discovered advertisementRef: Windows discovered advertisement
- Related peer_to_peer_server_ota firmware attached here for reference(7zip need to extract same).
- Related sniffer based packet info:

image.png



2. SDK has not a single STM32WBA52 BLE examples.

This topic has been closed for replies.

14 replies

STTwo-32
ST Technical Moderator
Aug 12, 2024 9:11 AM UTC

Hello @rajdeep_01 

Do you have the same behavior if you use one of the examples available for the STM32WBA52 Nucleo Board (Just download the version 1.1.0 of the STM32CubeWBA unzip it and open one of the examples available on this version using the STM32CubeIDE, compile and upload it). If you still have the same issue please report. I'm not able to reproduce the same issue on my side.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Aug 12, 2024 9:33 AM UTC

Hi @STTwo-32 

Thanks for update,
After initiated query in forum, already tried with different SDKs,
Facing same issue with below SDKs:
V1.4.0, V1.3.1, V1.3.0 and V1.2.0
Got success and everything working fine in below SDK:
V1.1.1.

As a workaround, can go with SDK V1.1.0 (4 Sep 2023 released),
but It will be great, if found fix to use latest SDK also.

Regards,
Rajdeep

STTwo-32
ST Technical Moderator
Aug 12, 2024 9:35 AM UTC

As you can see on the release note for the projects of the STM32CubeWBA V1.4.1:

  • Connectivity applications are not supported on this release for NUCLEO-WBA52CG board.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Sep 11, 2024 5:26 AM UTC

Hi @STTwo-32

Thanks for information, but main concern is related to MCU STM32WBA52CGU6 facing issue when incorporate SDK released after V1.1.1. Request STM-Team to fix the issue.

Note that STM claims that MCU STM32WBA52CGU6 has 10 year production support, I am assuming that STM will also support SDK releases during this timeline. Mark if any correction is there. 
It's strange that NUCLEO-WBA52CG has become overnight obsolete, even used MCU STM32WBA52CGU6 has 10 year production support.

Waiting for issue fix.

Regards,
Rajdeep

STTwo-32
ST Technical Moderator
Sep 11, 2024 6:19 AM UTC

Hello @rajdeep_01 

For the STM32WBA52 MCUs, they are available, and you can use them since they are supported by the Current SDK version. The only think is that Connectivity applications are not supported on this SDK release for NUCLEO-WBA52CG board. 

This product is obsolete, but you still can use the STM32WBA52 MCUs (As you already said, STM32WBA52 MCUs has 10-year production support). 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Sep 11, 2024 6:34 AM UTC

Hi @STTwo-32 

Thanks for quick reply, gained many information since ticket raised, but unfortunately looks like neither main issue is not properly addressed nor issue fix action initiated.

Let's focus on particular main concern:
STM32WBA52CGU6 Advertisement Issue: Discoverable in iOS/Windows not in Android.

Hope STM team will address main concern, proactive initiate action to fix issue and provide solution.

Regards,
Rajdeep