Question
STM32Cube_FW_WB: Applications fail to start because of assertion failure in APP_ZIGBEE_ConfigEndpoints
Multiple Zigbee examples in STM32Cube_FW_WB applications tree fail to start by triggering assertion failure in APP_ZIGBEE_ConfigEndpoints.
The code under questions is
static void APP_ZIGBEE_ConfigEndpoints(void)
{
struct ZbApsmeAddEndpointReqT req;
struct ZbApsmeAddEndpointConfT conf;
memset(&req, 0, sizeof(req));
/* Endpoint: SW1_ENDPOINT */
req.profileId = ZCL_PROFILE_HOME_AUTOMATION;
req.deviceId = ZCL_DEVICE_ONOFF_SWITCH;
req.endpoint = SW1_ENDPOINT;
ZbZclAddEndpoint(zigbee_app_info.zb, &req, &conf);
assert(conf.status == ZB_STATUS_SUCCESS);
...
}conf structure is not initialized, and it seems ZbZclAddEndpoint does not touch it at all leaving status member as is, causing the assertion to fail.
This problem is observed in multiple applications, OnOff_{Server,Client}_Distributed, OnOff_Client_Router and OnOff_Server_Coord. Other applications are very likely to have to the same problem.