cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding STM32WLE5JC Micro Controller interfacing with CAN: How to interface CAN protocol to STM32WLE5JC board. which module is suitable for communicating from STM32WLE5JC to CAN Protocol.

AA.21
Associate II

As of now, I work with the STM32WLE5JC controller. in that I need to interface CAN protocol for STM32WLE5JC board-to-board communication. For this is there any library available for this specific STM32WL controller and also which CAN module is suitable for interfacing with the STM32WL microcontroller.  kindly guide me on this.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
JMate.3
Associate II

Dear @AA.21​ 

There is a seeedstudio solution that you could use as reference

https://www.seeedstudio.com/LoRa-E5-CAN-FD-dev-kit-CANBUS-p-5398.html

AA.21
Associate II

I need to integrate STM32WL board to board communication by using external CAN bus module. So, Can you please suggest the suitable external CAN bus module (CAN controller +CAN transceiver integrated module) which provides UART interface to connect with STM32WL MCU?