Skip to main content
MLancaster
Visitor II
January 4, 2021
Question

Receiving HCI_HARDWARE_ERROR_EVENT from BLE Stack

  • January 4, 2021
  • 0 replies
  • 748 views

MCU: STM32WB55

BLE: BLE Stack Full V1.8.0

Hello,

I am using STM's BLE OTA example project (bootloader) and have it working with my custom firmware. I have noticed an issue that happens when updating my custom firmware via ota. Every so often I am unable to connect to the BLE_OTA firmware to download a new application. I was able to debug the BLE_OTA and find that the firmware acts up when an error event (HCI Event) is received.

I have noticed power cycling the MCU fixes the issue and the BLE OTA is able to function correctly. If I perform a software reset via NVIC_SystemReset() the BLE_OTA will run and Advertise BLE Data for maybe 10 seconds until receiving the error event again. I would like to fix this issue without power cycling the MCU.

Error Description found in Doc AN5270 Section 3.1 and 3.1.4

HCI_HARDWARE_ERROR_EVENT with error code 0x02 (event_time_overrun err)

I was wondering if anyone knows of any potential fixes, where I can find more information on the cause of the error event or what could potentially cause the error event.

Thank you for your help in advance.

This topic has been closed for replies.