Skip to main content
Andrew Neil
Super User
January 22, 2021
Question

P-Nucleo-LRWAN2 stops working on TTN

  • January 22, 2021
  • 2 replies
  • 1366 views

Cross-post on The Things Network (TTN) forum:

https://www.thethingsnetwork.org/forum/t/st-p-nucleo-lrwan2-stopped-working

I followed the 'Getting Started' instructions:

UM2587 Getting started with the P-NUCLEO-LRWAN2 and P-NUCLEO-LRWAN3 starter packs 1.0

It was all working on Tuesday (19th).

I could see traffic in the Gateway console view, and in the Device console view:

0693W000007CKsFQAW.png 

On the I-Nucleo-LRWAN1 device, the green LED blinks each time it transmits - I could see that a new payload appeared in the Device console view corresponding to each blink.

Some time in the latter part of Wednesday (20th), I noted that the LED had stopped blinking.

Investigating on Thursday (21st), looking at TTN Console, I saw that the Gateway status was ‘Not Connected’, and there was no data in the Device view.

I tried restarting the Gateway (AT+RESET), but that made no difference.

I found TTN forum posts saying that ‘Not Connected’ could simply mean that there’s no data going through the Gateway.

So I power-cycled the I-Nucleo Device.

This did start the LED blinking again, but TTN Console views showed only Join requests - no actual data messages:

0693W000007CKw7QAG.png 

The Gateway did seem to be sending Join accepts, but the device never seemed to see them - it just carried on sending requests.

Another TTN forum post mentioned that the device message counters might be out-of-sync - so I did a ‘Reset Frame Counters’ on the Device Overview console page:

0693W000007CKzpQAG.pngThis made no difference.

A different device (WizziLab SH2050 shield, in LoRaWAN mode) was able to join & send data OK.

So I left everything powered-up for a while - and it just started working again later in the day (Thursday).

This morning (Friday, 22nd), I see that the I-Nucleo has stopped blinking again!

(the WizziLab is still working).

The kit is all as-received - no configuration changes or firmware updates (other than as described in UM2587).

As supplied, the I-Nucleo blinks the green LED (ie, transmits?) every ~ 40s.

Is this too much? Could TTN be “blacklisting�? it, or something?

Another TTN forum post said it's important to keep the Device >8 feet from the gateway (to avoid cross-talk, interference, etc).

Mine was initially under 1 foot, but moving it to >12 feet away has made no difference:

The LD2 blue LED on the Gateway NUCLEO-F746ZG board blinks shortly after each blink of the I-Nucleo green LED (also after sending from the WizziLab device).

I haven’t seen a description of exactly what this indicates, but it seems to show that the Gateway at least thinks it has sent a reply?

Is there any way to get logs/diagnostics from the Gateway to see what's going on?

Likewise for the I-Nucleo.

Any other suggestions on what's going on here, or how to debug it?

I have already requested Gateway documentation - but no replies yet:

https://community.st.com/s/question/0D53W00000VgFJeSAN/pnucleolrwan2-gateway-documentation

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
January 22, 2021

Update from TTN forum:

While the I-Nucleo-LRWAN1 is in this state of not seeing Join Accepts:

0693W000007COOTQA4.pngThe Gateway is always sending its Join Accepts on 869.525, but the I-Nucleo sends its Requests on various frequencies. This is correct behaviour for the EU868 join RX2 window, which uses fixed settings

But TTN normally uses non-standard RX2 settings of SF9BW125 for non-join traffic - so could it be that the I-Nucleo is mistakenly also using SF9BW125 because it's on TTN, rather than reverting to standard for the TTN "special case" of joining?

https://www.thethingsnetwork.org/forum/t/st-p-nucleo-lrwan2-stopped-working/43127/10?u=dashcanttn

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
January 23, 2021

The fact that the WizziLabs devices work fine suggests that the problem lies in the I-Nucleo-LRWAN1 - not the gateway, or elsewhere in the network?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.