P-NUCLEO-LRWAN2 Gateway Board Stuck at "Ethernet Starting"
- 3 replies
- 546 views
Hello,
I am using the P-NUCLEO-LRWAN2 board for LoRaWAN development. While booting up the Gateway, it always gets stuck at the message
Powered by RisingHF & STMicroelectronics
-------------------------------------------------------------------------------
VERSION: 2.1.7, Nov 6 2018
LOG: OFF
AT ECHO: ON
BAUDRATE: 115200bps
MACADDR: 08:00:27:0C:23:38
ETHERNET: DHCP
DNS1: 114.114.114.114
DNS2: 8.8.8.8
NTP SERVER: 1.ubuntu.pool.ntp.org
EUI PADDING: {3, FF}, {4, FF}
GATEWAY ID: 080027FFFF0C2338
LORAWAN: Public
LORAWAN SERVER: router.eu.thethings.network
UPLINK UDP PORT: 1700
DOWNLINK UDP PORT: 1700
CHANNEL0: 867100000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL1: 867300000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL2: 867500000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL3: 867700000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL4: 867900000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL5: 868100000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL6: 868300000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL7: 868500000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL8: 868300000, B, SF7, BW250KHz (LORA_STANDARD)
CHANNEL9: 868800000, B, 50Kbps (FSK)
-------------------------------------------------------------------------------
Concentrator starting...
Concentrator Radio A type SX1257
Concentrator Radio B type SX1257
Concentrator started (2926ms)
ST LoRa GW V2
Ethernet starting...
After this point, the board does not proceed further.
Troubleshooting Done:
Tried rebooting multiple times.
Verified network cable and DHCP server are working fine.
Tried connecting to different routers/networks.
Reflashes firmware with the same version.
Board Details:P-NUCLEO-LRWAN2
I am not sure if this is an issue with firmware, hardware, or network configuration. Could you please help me troubleshoot or suggest further debugging steps?
Thank you.
Regards,
Hari Prasath P
Firmware Engineer
Senstornet Technologies
Chennai - India