Skip to main content
Andrew Neil
Super User
October 12, 2021
Solved

Full example/tutorial for I-CUBE-LRWAN v2.1.0 and The Things Stack (TTN v3) ?

  • October 12, 2021
  • 1 reply
  • 2087 views

I see there is now a video series on connecting the STM32WL to The Things Stack (TTN v3):

But this is specific to the WL, using the STM32CubeWL Pack.

Is it the same for the latest I-CUBE-LRWAN v2.1.0 ?

Specifically, on a B-L072Z-LRWAN1.

In particular, the video uses the WL's hardware ID register - so how would this be handled on the B-L072Z-LRWAN1 ?

This topic has been closed for replies.
Best answer by Andrew Neil

"But this is specific to the WL, using the STM32CubeWL Pack"

Also specific to TTN in North America.

That is to say, I tried it here in Europe, and the TTN Console operations are very different to those shown on the video - it's basically all the same bits of information, but very differently arranged on the screens.

TBF, I don't know if that's entirely an EU vs USA difference, or if the video is just out-of-date already and TTN have updated their screens & process.

We could certainly do with an EU version of the videos.

To answer my own questions:

"Is it the same for the latest I-CUBE-LRWAN v2.1.0 ?"

Yes, it does seem to be.

"the video uses the WL's hardware ID register - so how would this be handled on the B-L072Z-LRWAN1 ?"

It uses the STM32's MCU ID.

(Alternatively, I think TTN can generate a DevEUI?)

Conclusion:

Yes, following these videos (in particular, the 3rd one) will get you up and running with the End Node project on a  B-L072Z-LRWAN1 talking to The Things Stack (TTN v3).

:beaming_face_with_smiling_eyes:

1 reply

Andrew Neil
Andrew NeilAuthorBest answer
Super User
October 18, 2021

"But this is specific to the WL, using the STM32CubeWL Pack"

Also specific to TTN in North America.

That is to say, I tried it here in Europe, and the TTN Console operations are very different to those shown on the video - it's basically all the same bits of information, but very differently arranged on the screens.

TBF, I don't know if that's entirely an EU vs USA difference, or if the video is just out-of-date already and TTN have updated their screens & process.

We could certainly do with an EU version of the videos.

To answer my own questions:

"Is it the same for the latest I-CUBE-LRWAN v2.1.0 ?"

Yes, it does seem to be.

"the video uses the WL's hardware ID register - so how would this be handled on the B-L072Z-LRWAN1 ?"

It uses the STM32's MCU ID.

(Alternatively, I think TTN can generate a DevEUI?)

Conclusion:

Yes, following these videos (in particular, the 3rd one) will get you up and running with the End Node project on a  B-L072Z-LRWAN1 talking to The Things Stack (TTN v3).

:beaming_face_with_smiling_eyes:

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.