Skip to main content
Stecklo
Senior
November 6, 2019
Solved

Failed to read memory after RDP set/reset

  • November 6, 2019
  • 2 replies
  • 1970 views

I'm trying to program BLE stack on a custom board based on STM32WB55CG. I'm using SWD, CubeProgrammer 2.2, CubeFW_WB 1.1.1.

First I've successfully performed -fwdelete. But then I got "Firmware not authentic" error trying to make -fwupgrade. So I've set RDP 0xBB and back to 0xAA folowing this advice . And now I'm just unable to read or download anything except option bytes.

STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.2.0
 -------------------------------------------------------------------
 
ST-LINK SN : 066EFF393738425043094308
ST-LINK FW : V2J33M25
Voltage : 2.38V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
 
 
UPLOADING OPTION BYTES DATA ...
 
 Bank : 0x00
 Address : 0x58004020
 Size : 104 Bytes
 
██████████████████████████████████████████████████ 100%
 
 
PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: nboot0, value: 0x1, was not modified.
Warning: Option Byte: nboot1, value: 0x1, was not modified.
 
 Bank : 0x00
 Address : 0x58004020
 Size : 104 Bytes
 
██████████████████████████████████████████████████ 100%
 
Reconnecting...
Reconnected !
 
 
UPLOADING OPTION BYTES DATA ...
 
 Bank : 0x00
 Address : 0x58004020
 Size : 104 Bytes
 
██████████████████████████████████████████████████ 100%
 
OPTION BYTE PROGRAMMING VERIFICATION:
 
Option Bytes successfully programmed
 
 
Old Firmware delete ...
 
 
 
Memory Programming ...
Opening and parsing file: FUS_Operator.bin
 File : FUS_Operator.bin
 Size : 16882 Bytes
 Address : 0x08000000
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 4]
Download in Progress:
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒
 
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:00:00.721
 
 
 
Verifying ...
 
 
Read progress:
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒
 
Error: Failed to read memory at address 0x08000000 during verification
 
 
Error: Download verification failed
 
 
Error: Failed to download FUS operator!
STM32_Programmer_CLI.exe -c port=swd mode=UR -ob displ
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.2.0
 -------------------------------------------------------------------
 
ST-LINK SN : 066EFF393738425043094308
ST-LINK FW : V2J33M25
Voltage : 2.47V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
 
 
UPLOADING OPTION BYTES DATA ...
 
 Bank : 0x00
 Address : 0x58004020
 Size : 104 Bytes
 
██████████████████████████████████████████████████ 100%
 
 
OPTION BYTES BANK: 0
 
 Read Out Protection:
 
 RDP : 0xAA (Level 0, no protection)
 
 BOR Level:
 
 BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
 
 User Configuration:
 
 nBOOT0 : 0x1 (nBOOT0=1)
 nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
 nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
 SRAM2RST : 0x1 (SRAM2 is not erased when a system reset occurs)
 SRAM2PE : 0x1 (SRAM2 parity check disable)
 nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
 nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
 nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
 WWDGSW : 0x1 (Software window watchdog)
 IWGDSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
 IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
 IWDGSW : 0x1 (Software independent watchdog)
 IPCCDBA : 0x3FFF (0x3FFF)
 
 Security Configuration Option bytes:
 
 ESE : 0x1 (Security enabled)
 SFSA : 0x0 (0x0)
 FSD : 0x0 (System and Flash secure)
 DDS : 0x1 (CPU2 debug access disabled)
 C2OPT : 0x1 (SBRV will address Flash)
 NBRSD : 0x0 (SRAM2b is secure)
 SNBRSA : 0x0 (0x0)
 BRSD : 0x0 (SRAM2a is secure)
 SBRSA : 0x0 (0x0)
 SBRV : 0x3FC00 (0x3FC00)
 
 PCROP Protection:
 
 PCROP1A_STRT : 0x1FF (0x8000FF8)
 PCROP1A_END : 0x0 (0x8000008)
 PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
 PCROP1B_STRT : 0x1FF (0x8000FF8)
 PCROP1B_END : 0x0 (0x8000008)
 
 Write Protection:
 
 WRP1A_STRT : 0xFF (0x807F800)
 WRP1A_END : 0x0 (0x8000000)
 WRP1B_STRT : 0xFF (0x807F800)
 WRP1B_END : 0x0 (0x8000000)

This topic has been closed for replies.
Best answer by Remi QUINTIN

>I'm using SWD, CubeProgrammer 2.2, CubeFW_WB 1.1.1.

Please use the latest FW Package 1.3.0 at least to have the correct FUS and RF stack.

>STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0

Before launching this command, please be use to have issued a FWdelete command

Now the SFSA to 0 is showing a bloked board!!!

2 replies

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
November 6, 2019

>I'm using SWD, CubeProgrammer 2.2, CubeFW_WB 1.1.1.

Please use the latest FW Package 1.3.0 at least to have the correct FUS and RF stack.

>STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0

Before launching this command, please be use to have issued a FWdelete command

Now the SFSA to 0 is showing a bloked board!!!

Stecklo
SteckloAuthor
Senior
November 6, 2019

Thanks. If somebody would end up in similar situation here is the more specific discussion