Associate II
May 19, 2023
Solved
Fail to download code to the STM32WB55RG board using ST-link on STM32CubeIDE
- May 19, 2023
- 7 replies
- 4359 views
Hi,
Bought a new STM32WB55RG development board, created a sample code on STM32CubeIDE V1.12.1, compile good in IDE. ( using Windows 10)
But when download to the board by click the RUN button, it will pop up Error screen - The exception unknown software exception (0x40000015) occurred in the application at location 0x00000000000482646.
Created another example code, it had the same issue..
The board connect OK to Windows PC USB. I try another code and run on Keil, it does able to download. So I think the board itself is good, only the setting of the CubeIDE issue.
USB cable is only 2 feet long.
Thanks idea of to fix it?
thanks!