Skip to main content
Associate II
Jan 29, 2026 9:28 AM UTC
Question

Enrolling P-NUCLEO-LRWAN3 on Loriot Server

I have enrolled the gateway and the end node of my PNUCLEO lrwan 3 on Loriot server, but when I view the boot log on my Terra Term terminal, I observe that the end node does not join the server, returning JOINED FAILED.

I made sure the end node and the gateway are configured to the same frequency - EU433

I also made sure I used the correct details like the dev EUI, APP EUI amd AppKey from the end node to connect to the server, what could be the cause of this JOIN FAILED.

Screenshot (64).png

3 replies

Andrew Neil
Super User
Jan 29, 2026 9:36 AM UTC

As already noted, the P-NUCLEO-LRWAN3 gateway is obsolete - are you sure it is even supported by LORIOT now?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
027iconicAuthor
Associate II
Jan 29, 2026 11:24 AM UTC

The gateway firmware for Loriot server is still marked active on the PNUCLEO LRWAN 3 page so, I guess it is still supported by LORIOT.

Gatewayfirm.PNG

Andrew Neil
Super User
Jan 29, 2026 12:02 PM UTC

You should really confirm that with LORIOT...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.