Skip to main content
JSing.7
Visitor II
February 23, 2023
Solved

Does the STM32WB55RG micro controller chip offer inbuilt WiFi module?

  • February 23, 2023
  • 1 reply
  • 1085 views

..

This topic has been closed for replies.
Best answer by Peter BENSCH

As also mentioned on the STM32WB55RG website, the device contains a Cortex-M4 for user applications and is equipped with a 2.4GHz radio and the corresponding Cortex-M0, which can cover BLE 5.3, 802.15.4, Zigbee, Thread or Matter; WiFi is not included.

Does it answer your question?

Regards

/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
February 23, 2023

As also mentioned on the STM32WB55RG website, the device contains a Cortex-M4 for user applications and is equipped with a 2.4GHz radio and the corresponding Cortex-M0, which can cover BLE 5.3, 802.15.4, Zigbee, Thread or Matter; WiFi is not included.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.