Skip to main content
ashkanr65
Associate II
April 17, 2020
Solved

Connection problem for new board design

  • April 17, 2020
  • 1 reply
  • 942 views

I designed new board with STM32WB55CGU6 based on MB1993C (P-NUCLEO-USBDongle). You can see my schematic attached(I uploaded both P-nucleo schematic and my schematic). But I can't connect to my MCU through SWD pins (DIO,CLK,NRST). I use st-link, I can connect to P-nucleo usbdongle with these 3 pins, but I can't connect to my MCU. ST-Link can't find MCU. Unfortunately one of the crystals in my design (which is connected to pins number 23 and 24) has wrong footprint, but at least I should be able to connect to the MCU. does anyone know what is the problem?

This topic has been closed for replies.
Best answer by Tesla DeLorean

Make sure you provide a common ground.

The standalone ST-LINK/V2 (authentic) will also need VCC to pin 1.

If the IC is non-responsive​ need to focus on power and orientation. Check net list for disconnected or misnamed power nets.

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
April 17, 2020

Make sure you provide a common ground.

The standalone ST-LINK/V2 (authentic) will also need VCC to pin 1.

If the IC is non-responsive​ need to focus on power and orientation. Check net list for disconnected or misnamed power nets.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..