Skip to main content
Visitor II
September 3, 2023
Question

Can STM32WLE5CCU6 upport Wi SUN (IEEE802.15.4g in PHY layer) ?

  • September 3, 2023
  • 2 replies
  • 1343 views
I would like to inquire about something, such as the STM32WLE5CCU6 chip, which supports GFSK, but the chip manual does not explicitly state that it supports IEEE802.15.4g (for example, the s2 lp manual states that it supports IEEE 802.15.4g hardware package support with whitening, FEC, CRC, and dual SYNC word detection)
Can STM32WLE5CCU6 still support Wi SUN? Or can we only support IEEE802.15.4g through software?
This topic has been closed for replies.

2 replies

Issamos
Super User
September 3, 2023

Hello @coolliu 

As indicated in ST website, the only product that support WI-SUN is the S2-LP. That's why STM32WLE5CCU6 doesn't support it and may support the IEEE802.15.4g through software.

If this answer your question, please check this answer as best answer to be diffused.

Best regards.

II

 

Associate II
June 25, 2024

Does STM have IEEE802.15.4g stack implemented in any form ?