Bootloader to update firmware via UART: It is possible to invert UART TX pin?
My project requires a RS-232 cable with TX inverted to connect the PC with CubeProgrammer CLI to STM32WB55. In application, I am able to configure the UART with "UART_ADVFEATURE_TXINVERT_INIT", and the STM32WB55 transmission works fine through the RS-232 cable, but does not work on bootloader, since by default the TX pin is not inverted.
Any idea on how to workaround this?
A custom bootloader is an option to consider, but since I am using CubeProgrammer I would like to use the default bootloader from ST.